cancel
Showing results for 
Search instead for 
Did you mean: 

Stm32mp2 Android Problem with repo sync

dam_ourbot
Associate II

hi st team 

my environnement i use that : virtual box / ubuntu 24.0.0 / git 2.43.0  and repo 2.52

i follow this wiki https://wiki.stmicroelectronics.cn/stm32mpu/wiki/STM32MPU_Distribution_Package_for_Android

 

when i execute "repo sync" i have error on all github of stm32 repository  :

device-stm-openocd: fatal: not repository  git : '/home/linux/android/.repo/projects/device/stm/stm32mp2-openocd.git' device-stm-openocd: sleeping 4.0 seconds before retrying fatal: ce n'est pas un dépôt git : '/home/linux/android/.repo/projects/device/stm/stm32mp2-openocd.git' error: Cannot fetch device-stm-openocd from https://github.com/STMicroelectronics/device-stm-openocd Fetching: 100% (1/1), done in 4.100s Fetching: 0% (0/1) 0:04 | 1 job | 0:04 device-stm-openocd @ device/stm/stm32m.. fatal: ce n'est pas un dépôt git : '/home/linux/android/.repo/projects/device/stm/stm32mp2-openocd.git' device-stm-openocd: fatal: ce n'est pas un dépôt git : '/home/linux/android/.repo/projects/device/stm/stm32mp2-openocd.git' device-stm-openocd: sleeping 4.0 seconds before retrying fatal: ce n'est pas un dépôt git : '/home/linux/android/.repo/projects/device/stm/stm32mp2-openocd.git' error: Cannot fetch device-stm-openocd from https://github.com/STMicroelectronics/device-stm-openocd Fetching: 100% (1/1), done in 4.060s error: Cannot checkout device-stm-openocd: ManifestInvalidRevisionError: revision refs/tags/st-android-13.0.0-2024-07-31 in device-stm-openocd not found Checking out: 0% (0/1), done in 0.024s error: in sync device-stm-openocd: revision refs/tags/st-android-13.0.0-2024-07-31 in device-stm-openocd not found

So when i try git clone this repository  is work "git clone https://github.com/STMicroelectronics/device-stm-openocd "

In the manifest https://github.com/STMicroelectronics/android-manifest/blob/default/stm32mp2droid.xml 

have you same error ? 

 

Best regard 

 

 

 

 

 

 

 

 

 

 

 

 

2 REPLIES 2
Nicolas L
ST Employee

Hi

Just to be sure, did you set your $HOME/.netrc file with :

 machine github.com
 login "github login"
 password "github password"

See the information in the Wiki here after : https://wiki.st.com/stm32mpu/wiki/System_build_troubleshooting_grid

Regards

Nicolas

dam_ourbot
Associate II

Hi 

I created .netrc is work with my account github.

But i have same error : 

Fetching: 50% (1/2) 0:04 | 1 job | 0:03 stm32wrapper4dbg @ device/stm/stm32mp2..
fatal: ce n'est pas un dépôt git : '/home/linux/android/.repo/projects/device/stm/stm32mp2-openocd/stm32wrapper4dbg.git'

stm32wrapper4dbg:
fatal: ce n'est pas un dépôt git : '/home/linux/android/.repo/projects/device/stm/stm32mp2-openocd/stm32wrapper4dbg.git'
stm32wrapper4dbg: sleeping 4.0 seconds before retrying
fatal: ce n'est pas un dépôt git : '/home/linux/android/.repo/projects/device/stm/stm32mp2-openocd/stm32wrapper4dbg.git'
error: Cannot fetch stm32wrapper4dbg from https://github.com/STMicroelectronics/stm32wrapper4dbg
Fetching: 100% (2/2), done in 4.236s
info: A new version of repo is available
warning: repo is not tracking a remote branch, so it will not receive updates
================================================================================
Repo command failed: RepoUnhandledExceptionError
GitCommandError: 'reset --keep v2.53^0' on repo failed
stderr: error: Entry 'project.py' not uptodate. Cannot merge.
fatal: Impossible de réinitialiser le fichier d'index à la révision 'v2.53^0'.

 

i dont understand will when i try my envirronement repo with this project https://wiki.st.com/stm32mpu/wiki/STM32MPU_Distribution_Package and this line :

" repo init -u https://github.com/STMicroelectronics/oe-manifest.git -b refs/tags/openstlinux-6.6-yocto-scarthgap-mpu-v24.11.06"

" repo sync"

I dont have error , is work 

thanks for help