STM32 MPUs Software development tools

Ask questions and find answers on STM32 microprocessors software development tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 441 Views
  • 0 replies
  • 0 kudos

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 323 Views
  • 0 replies
  • 0 kudos

STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Resolved! How to enable 3 USB ports on STM32MP1

According to different STM32MP1 documentation such as STM32MP1-Peripheral-USB_Host_interface_USBH or STM32MP1-Peripheral-USB-On-The-Go-Full-and-HighSpeed-interface presentation there is two USB phy, one dual port HS phy and one single port FS phy. In...

PGE by Associate III
  • 5490 Views
  • 6 replies
  • 0 kudos

Yocto STM32MP157 DK2 - Display not working

HelloI use https://github.com/STMicroelectronics/meta-st-stm32mp with the stm32mp15-disco machine.It boots fine, I can access the shell via USB-UART. But the display just shows an STM Logo from the Bootloader. What do I need to change, so the display...

kbch by Associate III
  • 3726 Views
  • 4 replies
  • 0 kudos

Create new project in MX with STM32MP13

I have STM32CubeMX Version 6.10, STM32CubeIDE Version: 1.14.1with installed BSP STM32Cube_FW_MP13_V1.0.0When I create new bare project starting from evalboard STM32MP135F-DK as bare metal projectthen select NETXDUO, THREADX in Middleware and Software...

ravo_0-1710926926321.png ravo_1-1710926945424.png
ravo by Senior
  • 1538 Views
  • 1 replies
  • 0 kudos

STM32CubeIDE 1.15.1 released

STM32CubeIDE 1.15.1 was released on st.com as well as an in-tool update patch aligned with STM32CubeMX v6.11.1 that is available for download. Main issues fixed in this patch: Ticket 177978 : Fixed an issue with ST-LINK firmware upgrade concerning th...

information about file

Hi everyone,i am creating a custom machine on a STM32MP151CAA3T using mickledore as yocto layer.when i flash my image, the falshing stops on the first partition, when uses tf-a-usb.stm32 file.What is this file, how is generated and how i customize it...

Pavesino by Associate II
  • 1142 Views
  • 0 replies
  • 0 kudos