2023-04-26 9:45 AM
2023-10-11 3:09 AM
Hi,
I'd like to comment about ECC DDR3. This device can be used with standard SoC.
Please see below example based on Zentel Japan PN A3T4GF40CBF, 4Gb Built-in ECC DDR3/DDR3L SDRAM:
The ECC is a built-in function, the product has the features listed below
Note:
Alex
2023-04-27 8:18 AM
Hi @ABala.7
There is no support of DDR ECC on STM32MP1 products.
Regards,
In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'
2023-10-11 3:09 AM
Hi,
I'd like to comment about ECC DDR3. This device can be used with standard SoC.
Please see below example based on Zentel Japan PN A3T4GF40CBF, 4Gb Built-in ECC DDR3/DDR3L SDRAM:
The ECC is a built-in function, the product has the features listed below
Note:
Alex