STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! [secure boot] Is there a way to validate signed firmware externally (e.g without using BROM) ?

Hi,I'm following https://wiki.st.com/stm32mpu/wiki/STM32MP15_secure_boot tutorialI'd like to perform a few checks before programming OTP WORD 24 to 31 since, as usual, and as indicated in STM32MP1 reference manual:An OTP word can be written in multip...

aberdery by Associate II
  • 3218 Views
  • 2 replies
  • 0 kudos

Creating a bootable SD card with dd

I've tried to create a bootable CD card image using both the Starter image as well as a Yocto built image. In both cases the device fails to boot. I've gone into stm32mp1-openstlinux-4.19-thud-mp1-19-02-20/images/stm32mp1 directory and then run:scrip...

nlbutts by Associate II
  • 3658 Views
  • 3 replies
  • 0 kudos

Can't access "How to create a layer with device tree files generated via STM32CubeMX" page in Wiki

Hi,I'm going through the wiki to try and solve the issues I'm finding on the bring-up of our board.I found something that could be interesting for me , so from this page I try to access the "How to create a layer with device tree files generated via ...

j_gil by Associate II
  • 4310 Views
  • 8 replies
  • 0 kudos

root / ssh is wide open - no password

I connected my STM32MP1 via Ethernet to my network and was surprised that I could ssh root@192.168.x.ywithout a password. No password for root is a security risk. I immediately changed the root password to secure the device. Beware!-- John

JWali by Associate II
  • 1219 Views
  • 0 replies
  • 0 kudos

Resolved! STM32MP157C-DK2 won't boot after flashing

I'm able to download an image onto STM32MP157C-DK2 according to the wiki. The Cube Programmer indicates success. When I flip the boot switches to ON and reboot, DL8 lights after a few seconds but nothing on the screen. During flashing the LCD does di...

BMcCa.3 by Associate II
  • 5349 Views
  • 9 replies
  • 0 kudos