cancel
Showing results for 
Search instead for 
Did you mean: 

After update, AC6 SW4STM32 workbench version Java crash (Oct 10 2019)

debugging
Lead

Today got an update message in SW4 Eclipse to update Did that.

Now when trying to start "Debug" on an STM32MP1 board Exclipse just exits. The error is as follows. Debug files atttched.

Getting frustrated with the AC6/STM32MP1/Eclipse solution as a development environment ...Will go evaluate other platforms if the STM32MP1 environment and experience does not get stable soon.

OpenSTM32/plugins/com.st.stm32ide.mpu.externaltools.openocd.linux64_1.0.0.201902141520/resources/openocd-mpu/bin/openocd -d1 -f skeleton Debug (1).cfg -s /media/user/H3D1P2/Personal/2019/Projects/OpenSTM/Pangu/skeleton -s /media/user/H3D1P2/Tools/OpenSTM32/plugins/com.st.stm32ide.mpu.debug_1.1.0.201904120827/resources/openocd/st_scripts -c gdb_port 3333 -c tcl_port 6666 -c telnet_port 4444

#

# A fatal error has been detected by the Java Runtime Environment:

#

# SIGSEGV (0xb) at pc=0x00007f4b99aa973d, pid=19624, tid=0x00007f4bdd45a700

#

# JRE version: Java(TM) SE Runtime Environment (8.0_151-b12) (build 1.8.0_151-b12)

# Java VM: Java HotSpot(TM) 64-Bit Server VM (25.151-b12 mixed mode linux-amd64 compressed oops)

# Problematic frame:

# C [libgobject-2.0.so.0+0x3873d] g_type_check_instance_is_fundamentally_a+0xd

#

# Failed to write core dump. Core dumps have been disabled. To enable core dumping, try "ulimit -c unlimited" before starting Java again

#

# An error report file with more information is saved as:

# /media/user/H3D1P2/Tools/OpenSTM32/hs_err_pid19624.log

#

# If you would like to submit a bug report, please visit:

#  http://bugreport.java.com/bugreport/crash.jsp

# The crash happened outside the Java Virtual Machine in native code.

# See problematic frame for where to report the bug.

1 ACCEPTED SOLUTION

Accepted Solutions
debugging
Lead

For the record, cleaning up all my posts. Move to the IDE. CLOSED

View solution in original post

3 REPLIES 3
Olivier GALLIEN
ST Employee

Hi @debugging​ 

Problem probably come from an error during the Eclipse update process.

Could you please try to re-install from scratch ?

Note that tomorrow Friday the 11th of October will be release STM32CubeIDE V1.1.0 which will become the new reference IDE for MP1 development.

BR,

Olivier

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
debugging
Lead

That is excellent news! P.S: I went back to the previous version and that worked. Will try the the new IDE and also updated programmer.

debugging
Lead

For the record, cleaning up all my posts. Move to the IDE. CLOSED