cancel
Showing results for 
Search instead for 
Did you mean: 

CubeIDE v1.4.0 is not stopping on breakpoint

NGajic
Associate III

I'm trying to make FreeRTOS application which is involving ADC and sending messages via virtual UART to Cortex A7. So I began with example called OpenAMP_FreeRTOS_echo in the cube fw version 1.2.0. That example worked good. I saw echo on /dev/ttyRPMSG0. Then I tried to incorporate ADC into that code but without success (I made succes with ADC + virtual UART without using FreeRTOS, but I want to make FreeRTOS working). I had a lot of trouble using System Workbench in terms of ST-Link detection (I always had to change COM port in the Debug Configuration) and I read on this forum that there were troubles in using FreeRTOS and those troubles are solved in Cube IDE 1.2.1.

https://community.st.com/s/question/0D50X0000BI0vctSQB/freertos-does-not-run-on-stm32mp1-m4-core

So I recently switched to Cube IDE v1.4.0, but there I have trouble on stopping on breakpoint. I placed break point on lines after main which must be executed (i.e. HAL_Init), but the debug is not stopped.

Thanks in advance for the answer,

Nenad

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Olivier GALLIEN
ST Employee

Hi @NGajic​ 

In production mode, where M4 code is launched by A7, there is a delay between M4 core start and debugger attachment.

So all breakpoint set "too early" in the code are ignored.

Please confirm you can set breakpoint further in your code.

Usual tips to w/a this is either to add a sleep of few seconds at beginning of your main, or create while loop you can then bypass with debugger afterward.

Olivier

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
Olivier GALLIEN
ST Employee

Hi @NGajic​ 

In production mode, where M4 code is launched by A7, there is a delay between M4 core start and debugger attachment.

So all breakpoint set "too early" in the code are ignored.

Please confirm you can set breakpoint further in your code.

Usual tips to w/a this is either to add a sleep of few seconds at beginning of your main, or create while loop you can then bypass with debugger afterward.

Olivier

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
NGajic
Associate III

Hi OlivierG(iroud), :)

Thanx for your fast answer. Yeah, debugger stops after some time and I guessed that there is something in debugger. I will add delay.

Nenad