STM32 MPUs Boards and hardware tools

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STLINK-V3PWR quality control

Hello,The QC for STLINK-V3PWR assembled in France seems to be very bad. I received a unit that doesn't work out of the box (when USB is connected the status leds stay off, AUX power outputs 3.3V, host computer doesn't detect V3PWR).The same host comp...

JakaBac by Associate II
  • 2561 Views
  • 7 replies
  • 2 kudos

STM32MP1 pixel format RGB666

Hello,according to drivers/gpu/drm/stm/ltdc.c stm hardware supports these pixel formats:enum ltdc_pix_fmt {PF_NONE,/* RGB formats */PF_ARGB8888, /* ARGB [32 bits] */PF_RGBA8888, /* RGBA [32 bits] */PF_RGB888, /* RGB [24 bits] */PF_RGB565, /* RGB [16 ...

mishuk by Associate III
  • 1594 Views
  • 2 replies
  • 0 kudos

Display orientation

I am using the STM32MP157x-DK2 discovery board and building the qt-example image.During boot the ST splash screen is displayed on the LCD as things get underway. I replaced the .bmp with one of my own , horizontally oriented, and it was presented por...

LAK17AT by Associate II
  • 4025 Views
  • 3 replies
  • 0 kudos

Resolved! STM32MP157FAD1

Hello,I would like to ask you few questions since I have some unclearances about STM32MP157F MPU:1. If 933MHz DDR3L RAM was connected to the MPU according to the schematic, will the MPU automatically underclock it to max 533MHz?2. Is it possible to c...

filip1785 by Associate II
  • 1726 Views
  • 1 replies
  • 1 kudos