2023-09-01 1:45 PM
Solved! Go to Solution.
2023-09-06 1:07 PM
Thank you so much for the reply - Although very silly, your first suggestion turned out to help; I had confused "stm32mp15_st_common.h" with "stm32mp15_common.h" and edited the wrong one.
I still have problems, but I will add them in a separate post to stay on topic.
Thank you.
2023-09-02 3:20 AM
It appears that your modification to the U-Boot environment settings is not taking effect when U-Boot is launched. To troubleshoot this issue, you can follow these steps:
Double-check your modifications: Make sure you have saved your changes to the include/configs/stm32mp15_st_common.h file after adding the CONFIG_EXTRA_ENV_SETTINGS lines. Sometimes, changes might not be saved properly.
Rebuild U-Boot: After making changes to the U-Boot configuration, you should rebuild U-Boot to incorporate your modifications. You mentioned that you rebuilt the distribution (st-image-weston), but it's essential to ensure that U-Boot itself is rebuilt with your custom configuration. You can rebuild U-Boot by running the following command in your Yocto build environment:
This command will rebuild U-Boot with your custom environment settings.
Flash the modified U-Boot image: After rebuilding U-Boot, make sure that you flash the updated U-Boot image to the appropriate location on your STM32MP157D-DK1 board.
Confirm the environment variables: After flashing the updated U-Boot image, reboot your board and enter U-Boot. Then, check the environment variables to ensure that your changes are reflected:
This will display the current U-Boot environment variables, including bootcmd. Verify that your custom bootcmd is set correctly.
Save the environment: If you see that your custom bootcmd is correct but not taking effect, you may need to save the environment changes. You can do this by running the following command in U-Boot:
This command will save the current environment settings to non-volatile storage so that they persist across reboots.
Reboot the board: After saving the environment, you can reboot the board and see if your custom bootcmd is executed as expected.
If you follow these steps carefully and ensure that your custom bootcmd is set correctly in the U-Boot environment, it should work as intended. Make sure to double-check the U-Boot image's flash location and that your changes are saved correctly to the U-Boot environment
2023-09-06 1:07 PM
Thank you so much for the reply - Although very silly, your first suggestion turned out to help; I had confused "stm32mp15_st_common.h" with "stm32mp15_common.h" and edited the wrong one.
I still have problems, but I will add them in a separate post to stay on topic.
Thank you.