2023-01-06 1:20 AM
2023-01-06 5:29 AM
Hi @MAndreka ,
Could you please precise the application note you mentioned?
Is it AN5406: How to build a LoRa® application with STM32CubeWL.
If the answer is "yes", so the source codes are available in the package STM32CubeWL.
This later is available from following links:
I hope this answers your request.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-01-06 10:22 AM
I'm using an example app from STM32Cube_FW_WL_V1.3.0.FROM Projects>NUCLEO-WL55JC>Applications>SubGhz>SubGhz_Phy_PingPong.I'm using RM0453 Reference manual. I would like to use some of the commands from this ref man like :Set1TxParams() command. Now I would like library I should use, where do I get it and what header file I should include?Thanks.
Edited by moderation team to adhere the community guidelines.
2023-01-11 3:43 AM
Hi @MAndreka
Set TXParams(...) command is used to set the TX output power of Lora radio SX1261/62.
All SubGhz commands details are available in semtech datasheet which you can download from https://www.semtech.com/products/wireless-rf/lora-connect/sx1262.
STM32Cube_FW_WL_V1.3.0. has provided almost all the command support in radio driver so, no need any extra header or library. hope this will help