2024-02-16 02:59 AM - last edited on 2024-02-16 03:36 AM by Peter BENSCH
Hello,
I just came accross the STM32WL series and I was wondering if I can implement a different modulation other than the ones included (FSK, PSK).
I need to acquire an analog signal, convert it to digital and then modulate it with a frequency modulation and up-convert it and send it trough the PA. Can I do that using one of the STM32WL?
Thanks.
Solved! Go to Solution.
2024-02-16 03:53 AM
Hello @Jò and welcome to the ST Community :smiling_face_with_smiling_eyes:.
Our STM32WL series support LoRa, (G)FSK, (G)MSK and BPSK modulations. For more details, you can refer to the STM32WL documentations available on this link.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-02-16 03:53 AM
Hello @Jò and welcome to the ST Community :smiling_face_with_smiling_eyes:.
Our STM32WL series support LoRa, (G)FSK, (G)MSK and BPSK modulations. For more details, you can refer to the STM32WL documentations available on this link.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.