cancel
Showing results for 
Search instead for 
Did you mean: 

STM32WB5MMGH6 Project?

SWenn.1
Senior III

Hello.

I have done a few projects in the past with the above module and am currently working on a motor controller project using an X-NUCLEO-IHM03A and an NUCLEO-F401.  I want to know if the STM32WB5MMHG6 has enough room and power to integrate the motor controller application into the STM32WB5MMHG6 M4 core ?  Has anyone done this or can anyone point me to information regarding this?

 

Thanks

1 ACCEPTED SOLUTION

Accepted Solutions
STTwo-32
ST Employee

Hello @SWenn.1 

The capability to use a STM32WB on a motor control project may depend on the application characteristics. There is an example demonstrating how to spin a gimbal motor using STM32WB55 and ST's MCSDK v6 sensorless six-step algorithm: WB55Gimbal-6steps

So, this should be possible depending on the application. You may can give more details on your application and create a new post on the motor control forum to view the if it is possible or not.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
STTwo-32
ST Employee

Hello @SWenn.1 

The capability to use a STM32WB on a motor control project may depend on the application characteristics. There is an example demonstrating how to spin a gimbal motor using STM32WB55 and ST's MCSDK v6 sensorless six-step algorithm: WB55Gimbal-6steps

So, this should be possible depending on the application. You may can give more details on your application and create a new post on the motor control forum to view the if it is possible or not.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.