2022-06-28 8:23 AM
I have two P-Nucleo-WB boards and both of them end up in this state.
CubeIDE trying to load binary:
CubeProgrammer:
Found several topic that looks the same however nothing helped. Has anyone solved this problem?
2022-07-19 2:53 AM
Hello,
I think you should check in the device management if there is no problem with the ports, and try to disconnect the port in device management and reconnect.
Check if all jumpers are correctly configured :
Make sure to upgrade the ST-LINK/V2-1 firmware. Are you able to connect your board in USB DFU mode ? If yes, can you recover the option bytes please ?
Best Regards
2022-07-19 4:27 AM
This is how my Linux recognize device:
Jumpers are set up as you described. I can't connect by DFU:
2022-07-19 7:44 AM
Hello,
In order to connect the board using USB DFU mode, you must have the following configuration:
The following configuration is used to connect the board using ST LINK:
Best Regards
2022-07-19 9:37 AM
Hi Remy,
I was able to connect with USB DFU mode however I don't know how to recover option bytes. Could you please tell me how to do that?
Best regards
2022-07-20 3:19 AM
Hello,
Can you try to connect your board to STM32CubeProgrammer using ST LINK by following these steps ?
Best Regards
2022-07-20 4:13 AM
make sure your power supply is good then you should try. i think your problem is form power supplier or low voltage system.
2022-07-20 6:46 AM
Are you using an unpowered hub to connect to the board to?
I plug mine directly into the computer.
I have also had luck with a powered USB 3.1 Hub. The powered hub has its own power supply and does not pull power from the PC. Mine is an Inland 7 port hub with a 2000 mA power supply. It has no model number on the case.
I got it from Microcenter here is a link:
2022-07-25 2:19 PM
Hi Remy,
Don't worry about it, you're fine. The last time I bricked something was about four years ago. When I first used this product, I thought that my cell phone would blow up. Can it be recovered?
Best regards
2022-07-31 1:18 PM
Hi All,
Thanks for all your replies. I have tested voltages with few chargers and still got this same result.Tested both ports: USB MCU and ST-LINK (jumpers in correct settings). I am not using any USB hub. I used to plug it directly to laptop - laptop voltage is ok (5V).
@Remy ISSALYS
Tried to connect they way you said but it still fails: Error: No STM32 target found!