cancel
Showing results for 
Search instead for 
Did you mean: 

STM32WB Thread-RCP and Raspberry Pi 3B for Border Router feature.

YTalh.1
Associate II

From the STM32CubeWB firmware package, there is a Thread_RCP project. However, there doesn't seem to be any documentation for it (it is not even mentioned in AN5289). The only hint is the readme.txt file which says:

"This application is used to demonstrate the OpenThread Border router feature using an STM32WB device.

To play with the demo, you need a Raspberry Pi 3B (RPi) to perform the link with Wi-Fi/Ethernet networks

The full setup and the associated documentations can be requested to ST on demand".

Where can I find the full setup and associated documentation?

Thank you,

14 REPLIES 14

@Remi QUINTIN​ 

Appreciated if you can advise on this?

the document has 13 pages; just download it . :)

If you feel a post has answered your question, please click "Accept as Solution".

The documentation says this, so I'm asking.

​

A full configured RPi image is provided by ST.

Please get the OTBR_CLI_RPi_1.0.img.

​

Regards​

Mute pon., 21 lis 2022, 01:01 użytkownik ST Community napisał:
pczekalski
Associate

I'm also looking for the OTBR_CLI_RPi_1.0.img downloading sources for my students (educational HE project).

Is there any info I'm missing? All documentation links stating "get ... file" are inactive.

 

Best regards,

 

Piotr