2019-09-16 7:48 PM
I'm working with the p-nucleo-wb55, and I would like to configure the pin PA0 , PC13 to wake up the MCU from Standby Mode. I configued PA0 and PC13 from STM32CubeMX to GPIO_EXTI0 and GPIO_EXTI13 respectively.
Config:
PA0 : External Interrupt with Falling edge , Pull-up
PC13 : External Interrupt with Falling edge , Pull-up
In my code I set the sequence that I follow to enable the WKUP line is:
HAL_PWR_EnableWakeUpPin(PWR_WAKEUP_PIN1_LOW);
HAL_PWR_EnableWakeUpPin(PWR_WAKEUP_PIN2_LOW);
HAL_PWR_EnterSTANDBYMode();
But interrupt from PA0 , PC13 not working in standby mode.
I reference from
RM0434: Multiprotocol wireless 32-bit MCU Arm®-based Cortex®-M4 with FPU, Bluetooth® Low-Energy and 802.15.4 radio solution
2019-09-17 12:20 AM
Hello @jirdom ,
This does not exactly points to your solution but you can have a look inside the STM32Cube_FW_WB_V1.2.0 under Projects\P-NUCLEO-WB55.Nucleo\Examples\PWR.
You will find 5 examples detailing how to go to the various low power mode and use the various wake up sources:
Pierre.
2019-09-18 12:13 AM
Hi Le Corre Pierre(ST Employee)
Thank for your information.
Do have example wake up from standby mode with WKUPx?
I checked from stm32wb55rg datasheet (LINK) on page 35. Standby mode able to wakeup by RF, Reset pin 5 I/Os (WKUPx) BOR, RTC, IWDG.
And the I/Os with wakeup from Standby/Shutdown capability are: PA0, PC13, PC12, PA2, PC5
2020-09-07 11:12 PM
Hi JIrdom
Did you ever find solution to your problem? I can use the example PWR_STANDBY_RTC and wake up from rtc and wake up from wakeup pin with bare code.
But as soon as i add BLE funtionality wakeup pin does not work anymore. , but RTC wakeup works fine
2022-12-21 10:46 AM
Hello @jirdom and @HSpre.1 ,
I am working on a project with the STM32WB55xx MCU.
I was wondering, even a long time after, if you had found a solution to your problem. I encounter exactly the same situation and I don't know what to do. On the datasheet, ST says :
"Standby Mode - Wakeup capability : Radio system (Bluetooth Low Energy, 802.15.4) ".
But then I couldn't wake up the MCU with RF or even with the WKUPx pins.
If you have any idea I would really appreciate your help :)
Thank you very much,
Best regards,
Eloi B.
2024-12-13 6:07 AM
Hello @eloibonte @HSpre.1 @jirdom
I am working on a project with the STM32WB55
Even a long time after, I wondered if you had found a solution to your problem. I encounter the same situation and I don't know what to do.
I have a timer that after 5 sec launch the offmode :
HAL_GPIO_TogglePin(LD3_GPIO_Port, LD3_Pin);
count++;
if (count > 5)
{
count = 0;
//HAL_PWR_DisableWakeUpPin(PWR_WAKEUP_PIN1);
//HAL_PWR_DisableWakeUpPin(PWR_WAKEUP_PIN2);
//HAL_PWR_DisableWakeUpPin(PWR_WAKEUP_PIN3);
//HAL_PWR_DisableWakeUpPin(PWR_WAKEUP_PIN4);
HAL_PWR_DisableWakeUpPin(PWR_WAKEUP_PIN5);
/* Clear all related wakeup flags*/
__HAL_PWR_CLEAR_FLAG(PWR_FLAG_WU);
/* Enable WakeUp Pin PWR_WAKEUP_PIN2 connected to PC.13 */
//HAL_PWR_EnableWakeUpPin(PWR_WAKEUP_PIN1);
// HAL_PWR_EnableWakeUpPin(PWR_WAKEUP_PIN2);
//HAL_PWR_EnableWakeUpPin(PWR_WAKEUP_PIN3);
// HAL_PWR_EnableWakeUpPin(PWR_WAKEUP_PIN4);
HAL_PWR_EnableWakeUpPin(PWR_WAKEUP_PIN5);
PWR_EnterOffMode();
}
With this example, I do enter in Off mode (the Led stop to blink). But none (even if uncomment ) of the wake up pin work. (The led do not goes to blink)
But there are correctly set as you can see:
2025-01-20 9:50 AM - edited 2025-01-20 9:52 AM
Wonder if somebody found the solution.
I use the stm32wb with rf and uart (at least during debug stage) and have an external pull down on SYS_WKUP_4. A button will feed it with 3.3V/Vcc if it has to wakeup.
First problem is that I have to use HAL_SuspendTick(); to prevent the uart and most probably also the rf to interfere (otherwise it will not sleep and continue). next I use:
__HAL_PWR_CLEAR_FLAG(PWR_FLAG_WU);
HAL_PWR_EnableWakeUpPin(PWR_WAKEUP_PIN4);