2022-12-27 3:16 AM
Greetings,
Currently the project has a requirement for a Custom BLE server profile. I have a few doubts, for which I'm seeking clarifications.
Awaiting your response at the earliest.
Thanks,
Akash Bharadwaj
Solved! Go to Solution.
2022-12-27 6:00 AM
A quick answer:
Wen using CubeProgrammer to flash the device, you have to check the "Start Wireless stack" button to ensure the program counter of the M0+ cote (CPU2) is indeed set at the start of the wireless stack.
Otherwise the CPU2 will never execute the wireless part and instead will remain on the FUS. This can explain your second point as CPU2 when launched by CPU1 is not executing the right code.
2022-12-27 6:00 AM
A quick answer:
Wen using CubeProgrammer to flash the device, you have to check the "Start Wireless stack" button to ensure the program counter of the M0+ cote (CPU2) is indeed set at the start of the wireless stack.
Otherwise the CPU2 will never execute the wireless part and instead will remain on the FUS. This can explain your second point as CPU2 when launched by CPU1 is not executing the right code.
2023-01-03 9:23 PM
@Remi QUINTIN
Thanks for the update.