Skip to main content
Associate II
February 26, 2025
Solved

CUSTOM BOOTLOADER

 

ISSUE: STM32F7 Custom Bootloader - Main Application Not Running After Jump
Details:
Bootloader Memory Definition:

RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 320K
FLASH (rx) : ORIGIN = 0x8000000, LENGTH = 1024K
QUADSPI (r) : ORIGIN = 0x90000000, LENGTH = 16M

Application Memory Definition:

RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 320K

FLASH (rx) : ORIGIN = 0x8020000, LENGTH = 896K

QUADSPI (r) : ORIGIN = 0x90000000, LENGTH = 16M

Validation Points:
Bootloader erase & write operations are working correctly.
Custom bootloader successfully writes the application code to both internal and external segments.
A test application that prints text ("I am application") works properly after jumping from the bootloader.


Debug points :

1 > memory utilization by main application

RAM : ORIGIN = 0x20000000, utilization = 320 K

FLASH : ORIGIN = 0x8020000, utilization = 896 K

QUADSPI : ORIGIN = 0x90000000, utilization = 5.18 M

 

2 > Jump steps after writing application (by custom bootloader)

if(gParsePacketData.data[0] == BOOT_STATUS)
{

#define APP_ADDRESS 0x08020000 
typedef void (*pFunction)(void);
pFunction JumpToApplication;
uint32_t JumpAddress;
int Temp = 0 ;
vc_prepare_packet_and_send(&huart6,FEEDBACK_COMMAND,FEEDBACK_SUCCESS,&Temp,sizeof(Temp));


// Disable interrupts
 __disable_irq();

 // Deinitialize peripherals and clocks if needed

 // Set vector table to application address
 SCB->VTOR = APP_ADDRESS;

 // Read the application's stack pointer address
 __set_MSP(*(volatile uint32_t*)APP_ADDRESS);

 // Get the application's reset vector (entry point)
 JumpAddress = *(volatile uint32_t*) (APP_ADDRESS + 4);
 JumpToApplication = (pFunction) JumpAddress;

 // Enable interrupts (optional, the application should handle it)
 __enable_irq();

 // Jump to application
 JumpToApplication();

We would be grateful for any guidance or suggestions you can provide.

This topic has been closed for replies.
TDK
TDKBest answer
February 27, 2025

> The jump function works correctly when the application is downloaded using the STM32 Programming Utility, but it fails when the main application is downloaded via my custom application.

Suggests the bug is in your application download. Compare the flash between the two methods to find out what is different.

"If you feel a post has answered your question, please click ""Accept as Solution""."

10 replies

Karl Yamashita
Principal
February 26, 2025
  1. find system_stm32f7xx.c file
  2. Uncomment this define
  3. Change value to your application address

 

KarlYamashita_0-1740554407540.png

 

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.CAN Jammer an open source CAN bus hacking toolCANableV3 Open Source
Associate II
February 26, 2025

Vishwajeet_0-1740554948571.png

Vishwajeet_1-1740554977566.png

Thank you for your valuable reply, but the changes have already been made and tested.

SSten.1705
Associate
February 26, 2025

I am using a bootloader that checks checksum and jumps to it, using struct and code below. Make sure not to have any DMA or interrupts being active when jumping.

// Struct for relaxed addressing
typedef struct
{
 void *stack;					//0
 void (* appentry)(void);		//1
 u32 pad[5]; 					//2 3 4 5 6	
 void (* frestrict)(int code); 	//7
 u32 checksum;				//8
 u32 flashend; 				//9
 u32 version;				//10 0x08000028
} APPINFO;

// jump to application if valid
// called also after successfull firmware upgrade 

#define APPSTART 0x08020000

void checkapp(bool reset)
{
	u32 xs = 0;
	
	const u32 *bin = (u32 *)(APPSTART);
	
	const APPINFO *ai = (APPINFO *)bin;

	u32 fend = ai->flashend;
	
	if((fend < APPSTART) || (fend > 0x080E0000) )	return;	// should be reasonable, last sector for storage?
	
	while(bin < (u32 *)fend) xs += *bin++;
		
	if(xs == 0)
	{
		if(reset) ResetPeriph();
		ai->appentry(); 					// bye!
	}
}

I am  

Tesla DeLorean
Guru
February 26, 2025

On the app side, I would avoid doing any system clock (RCC) re-initialization, or that of the pins and the QSPI / External memory interfaces that the loader has already brought up to operational status.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
TDK
February 26, 2025

> A test application that prints text ("I am application") works properly after jumping from the bootloader.

If a test application works, but your main app doesn't, doesn't that suggest a bug with your main application? Certainly it means the jump is working as intended.

Debug the code, let the jump happen, pause the code and examine the state of the system. Could be that you're in an interrupt that now points to an invalid location. You don't actually disable any interrupts. Only temporarily.

How to jump to system bootloader from application ... - STMicroelectronics Community

"If you feel a post has answered your question, please click ""Accept as Solution""."
Tesla DeLorean
Guru
February 26, 2025

Prioritize getting working HardFault_Handler() and Error_Handler() in both loader and app, that can give visible and definitive information if they arrive there. For the latter a source file and line would help pin things down quickly.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
jumman_JHINGA
Senior III
February 27, 2025

Try this jump code:

void Jump_To_User_Application(void)
{

 // check if valid code is present on Application sector
 
 if((((*(__IO uint32_t*)APPLICATION_ADDRESS) & 0xFF000000 ) == 0x20000000) || \
 (((*(__IO uint32_t*)APPLICATION_ADDRESS) & 0xFF000000 ) == 0x10000000))
 {
 JumpAddress = *(__IO uint32_t*) (APPLICATION_ADDRESS + 4); // Take jump address from application sector
 Jump_To_Application = (pFunction) JumpAddress;

 /***************** Deinitialized every thing***************************/
 HAL_RCC_DeInit();
 HAL_DeInit();
 /* // This Commented part needed when if we are using timer or other interrupts
 for(int i=0;i<8;i++)
 {
 NVIC->ICER[ i ] = 0xFFFFFFFF ;
 NVIC->ICPR[ i ] = 0xFFFFFFFF ;
 }

 SCB->ICSR |= SCB_ICSR_PENDSTCLR_Msk ;
 
 SCB->SHCSR &= ~( SCB_SHCSR_USGFAULTENA_Msk | SCB_SHCSR_BUSFAULTENA_Msk | SCB_SHCSR_MEMFAULTENA_Msk ) ;
 */		 
 SysTick->CTRL = 0;
 SysTick->LOAD = 0;
 SysTick->VAL = 0;
 /******************Deinitialization end**********************************/
 SCB->VTOR = APPLICATION_ADDRESS; // Change Vector Table address with user application address
			 
 __set_MSP(*(__IO uint32_t*) APPLICATION_ADDRESS); // Set Main Stack Pointer to User Application address location
 Jump_To_Application(); // Jump to application usinf pFunction
 }
 
}