cancel
Showing results for 
Search instead for 
Did you mean: 

make: *** No rule to make target 'C:/Utilities/trace/adv_trace/stm32_adv_trace.c', ...

ledi001
Senior

Hi,

I have copied a sample project from STM32Cube_FW_WBA_V1.4.1 to another location.
After importing the project into CubeIDE1.16.1 and compiling it, I got the error message:

 

make: *** No rule to make target 'C:/Utilities/trace/adv_trace/stm32_adv_trace.c', needed by 'Utilities/stm32_adv_trace.o'.  Stop.

 

 After cleaning the project, same result. Can somebody help?

 

1 ACCEPTED SOLUTION

Accepted Solutions
ledi001
Senior

I solved the problem when i opend the regarding folder with "Open Projects from File System..."

View solution in original post

4 REPLIES 4
Souhaib MAZHOUD
ST Employee

Hello @ledi001 

Could you refer to this thread it could help you solve the issue!

KR,

Souhaib

Hello @Souhaib MAZHOUD 

i want to use the project BLE_p2pServer_ota for STM32WBA55 as template and expand it.

Therfore i have to copy the project in my SVN repository.

ledi001
Senior

Then i tried to export the project as archive file (.zip file) by using the export wizard and import it as "Existing Projects into Workspace" but i got the same error.

ledi001
Senior

I solved the problem when i opend the regarding folder with "Open Projects from File System..."