2024-11-15 6:40 AM
Hi, i have started testing the STM32WL Nucleo-64 with the Lorawan End Node Firmware. At first it seem to run OK, the device connects to the gateway and the data packets reach the platform i use. But the device stops working correctly with a few mwters of distance. I have seen that the BGS13S4N9 chip is not being powered, and the signals FE_CTRL1, FE_CTRL2 and FE_CTRL3 are always on reset state, though the firmware is setting them on.I have not modify the pinout or any configuration not needed. Is this a firmware configuration issue?
Kind Regards,
LuisL
Solved! Go to Solution.
2024-11-29 3:57 AM
Hi i have found the problem, i had the FE_CTRL pins not configured in stm32wlxx_nucleo_radio.h and stm32wlxx_nucleo_radio.c , now it works as intended
2024-11-25 12:59 AM
Hello @LuisL
I'm not able to reproduce this behavior. Could you try the same test using another NUCLEO-WL55JCx and see if you see the same behavior.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-11-29 3:57 AM
Hi i have found the problem, i had the FE_CTRL pins not configured in stm32wlxx_nucleo_radio.h and stm32wlxx_nucleo_radio.c , now it works as intended