cancel
Showing results for 
Search instead for 
Did you mean: 

How to add the custom service to the existing TMAP_Client code.

Pallavi
Associate III

Hi @STTwo-32 @KDJEM.1 
I want to add custom services along with the BLE_TMAP_Audio_Unicast_Client of STM32WBA55G-DK board. 

The .ioc file is already configured and I am not able to add more services. 
Can someone provide with CubeMX initialization for WBA. 

The user manual UM1718 has STM32WPAN section for STM32WB series only. UM3131 is also not helping with the need.

Thanks in advance!

1 ACCEPTED SOLUTION

Accepted Solutions
STTwo-32
ST Employee

Hello @Pallavi 

For the initialization of an application using the STM32WBA on CubeMX, I may recommand you to follow thos e two Wikis:

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

3 REPLIES 3
STTwo-32
ST Employee

Hello @Pallavi 

For the initialization of an application using the STM32WBA on CubeMX, I may recommand you to follow thos e two Wikis:

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

I am following these pages. 
https://wiki.st.com/stm32mcu/wiki/Connectivity:Bluetooth_LE_Audio_-_STM32WBA_Architecture_and_Integration this talks about audio integration. What if i have to integrate heart rate service along with it? 
How do I add that?

It is almost the same way as the first link I've mentioned to you.

Best Regards.

STTwo-32

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.