2024-02-22 08:54 AM
I am using the p-nucelo-lrwan3 and I have been using the i-cube-wl project and i did some changes to the region and to the activation mode but it doesn't join the network can any body help me with it
2024-02-26 08:46 AM
Hi there ,
i did connect an other end-node(with the default program) to my gateway and it work and i tried to connect my end-node and it didn't join
2024-02-26 09:06 AM
maybe your radio module is damaged. I suggest you to change it.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-02-26 10:36 AM
Yeah i thought that may be the radio module is damaged but even i used an other one but nothing change
2024-02-26 10:38 AM
Yeah i thought that may be the radio module is damaged but even i used an other one but nothing change
2024-02-26 10:40 AM
But you said that you have connected another node. Can you explain more.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-02-26 10:50 AM
Yes that's right,first i had connected an other node but it was the same as mine then i thought may be the module of my node is damaged so i changed it by the other node 's module but nothing changed
2024-02-26 10:54 AM
You can try to use your module with another board. If it works, Then the L0 of your node is damaged. Else, you need to use a new end node (board L0 and radio module).
Best Regards
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-02-27 06:23 AM
i have tried to load a simple blink led to my L0 and it work but i have found a file .bin (rhf0m003-v3.5.13.bin) in the risinghf site and when i try to drag and drop it in the L0 it failed
is there any solution exept getting a new end node
2024-02-27 06:56 AM
@Dan33 wrote:i have found a file .bin (rhf0m003-v3.5.13.bin) in the risinghf site
Here: https://www.risinghf.com/product/detail/19 ?
So have you contacted RisingHF Support:support@risinghf.com ?
@Dan33 wrote:when i try to drag and drop it in the L0 it failed
In what way(s), exactly, did it "fail" ?
2024-02-27 07:10 AM
acutely i haven't contacted RisingHF Support but i found the file in here :https://www.risinghf.com/product/detail/19
and by it failed i mean it failed to copy to the mass-storage device