cancel
Showing results for 
Search instead for 
Did you mean: 

End node stm32l073rz and lrwan-ns1 doesn't join

Dan33
Associate II

I am using the p-nucelo-lrwan3 and I have been using the i-cube-wl project and i did some changes to the region and to the activation mode but it doesn't join the network can any body help me with it 

20 REPLIES 20
Dan33
Associate II

Hi there ,

i did connect an other end-node(with the default program) to my gateway and it work and i tried to connect my end-node and it didn't join 

maybe your radio module is damaged. I suggest you to change it.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Dan33
Associate II
Yeah i thought that may be the radio module is damaged but even i used an other one but nothing change
Dan33
Associate II

Yeah i thought that may be the radio module is damaged but even i used an other one but nothing change

But you said that you have connected another node. Can you explain more.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Yes that's right,first i had connected an other node but it was the same as mine then i thought may be the module of my node is damaged so i changed it by the other node 's module but nothing changed 

You can try to use your module with another board. If it works, Then the L0 of your node is damaged. Else, you need to use a new end node (board L0 and radio module).

Best Regards

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Dan33
Associate II

i have tried to load a simple blink led to my L0 and it work  but i have found a file .bin (rhf0m003-v3.5.13.bin) in the risinghf site and when i try to drag and drop it in the L0 it failed 

is there any solution exept getting a new end node 

 

 


@Dan33 wrote:

 i have found a file .bin (rhf0m003-v3.5.13.bin) in the risinghf site


Here: https://www.risinghf.com/product/detail/19 ?

So have you contacted RisingHF Support:support@risinghf.com ?

 


@Dan33 wrote:

 when i try to drag and drop it in the L0 it failed 


In what way(s), exactly, did it "fail" ?

  • Failed to copy to the mass-storage device?
  • Failed to program the target microcontroller?
  • Failed to run after programming (give details) ?
  • other ?

 

 

Dan33
Associate II

acutely i haven't contacted RisingHF Support but i found the file in here :https://www.risinghf.com/product/detail/19

and by it failed i mean it failed to copy to the mass-storage device 

Dan33_0-1709046587380.png