cancel
Showing results for 
Search instead for 
Did you mean: 

BLE & Thread Concurrent project

romihs
Associate II

Is it possible to create a project in CubeMX for a concurrent BLE & Thread application for the STM32WB55?

My attempts so far only allow for either a BLE or a Thread project (not both together).

Thanks

1 ACCEPTED SOLUTION

Accepted Solutions
Remy ISSALYS
ST Employee

Hello,

Unfortunately, CubeMX tool doesn't support concurrent mode application.

Best Regards

View solution in original post

3 REPLIES 3
Imen.D
ST Employee

Hello @romihs​ and welcome to the Community :)

An example of concurrent mode (BLE/Thread) is provided in the STM32CubeWB firmware package.

I advise you to have a look at the available applications, which are located under: Projects\P-NUCLEO-WB55.Nucleo\Applications\ directory.

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
romihs
Associate II

Thanks @Imen DAHMEN​

Yes, I am aware of the projects in the STM32CubeWB package.

The reason I was asking was that I would like to start a clean project with both BLE and Thread, and was just wondering if it could be started from CubeMX...

Remy ISSALYS
ST Employee

Hello,

Unfortunately, CubeMX tool doesn't support concurrent mode application.

Best Regards