cancel
Showing results for 
Search instead for 
Did you mean: 

TouchGfx widget internet connectivity

DOkaz.1
Associate II

Hi,

I want to connect a display powered by TouchGFX to a PC via usb-c. Is it possible to allow internet connectivity for a GUI widget via the usb-c connection to the host PC?

Thanks!

1 ACCEPTED SOLUTION

Accepted Solutions
7 REPLIES 7
MM..1
Chief III

TouchGFX dont have prepared widget , but your code can use internet your way.

How would the widget connect to the internet? does the board require its own TCP/IP stack chip? or is there a way todo like REST API calls or some other way to communicate over the internet?

Just trying to figure out if there is some pre-existing infrastructure that I can use or if it would need to be coded from scratch. or require some external hardware

Thanks!

Piranha
Chief II

that looks like what I'm looking for, i'll look more into it. Thanks!

MM..1
Chief III

Why not board or STM with ethernet ? Is more simple as USB C

STM32 Nucleo Boards - STMicroelectronics

The usecase I have will only have a usb-c port as its interface, so having a full ethernet port would be a lot easier but wouldn't fit in the overall design

Then yes STM have in USB CDC ECM and NDIS... Examples on github