STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

New STM32F429I Discovery - Is my LCD damaged?

I just received my new STM32F429I Discovery board and I have uploaded the TouchGFX example.The LCD looks like clumsy at touch and the y axis is someway inverted.See my short video here (Unfortunately as new member I cannot add links, links are in the...

Fab64 by Associate
  • 1963 Views
  • 3 replies
  • 0 kudos

Resolved! Problem with Flex button in TouchGFX 4.21.2 Designer

I'm trying to use images through the flex button, but, when i select some images, there isn't any visual update and selection update. I tried change the "released" image and continuous with "No image" after the selection in my library images.anyone k...

FDigi by Associate III
  • 3752 Views
  • 5 replies
  • 1 kudos

STM32L4 OCTOSPI Memory Mapped Mode Failure Modes

Hi all,We are testing the failure modes for the OCTOSPI memory mapped mode and there isn't much info in the documentation.The setup:* STM32L4S9ZIJ6* Dual external RAM chips (CY15B104QSN) configured for dual QPI DTR.* External memory used for TouchGFX...

RRaak.1 by Associate II
  • 1887 Views
  • 1 replies
  • 0 kudos

Use of TouchGFX, Ethernet and LwIP on STM32H743 eval2, after setting up ETH, LwIP then downloading to eval2, screen unable to display

I create new project from touchGFX, by adding 5 simple widgets , generate code, run simulators, run targer all are working and success. Open the file with CubeIDE, build and run ars also OK.Enable and set up ETH, LwIP, freertos using CubeIDE are ok....

ET.2 by Associate III
  • 1760 Views
  • 1 replies
  • 0 kudos

Resolved! Scale Image when moving in a scrollwheel

Hi,I have a horizontal scrollwheel where i want to scale the item when it is animating to the next position. I am a bit lost how to start with this. I had a look at move animator but that doesn't seems like the proper way. I need a hook from the scro...

BNuyt.1 by Associate
  • 1427 Views
  • 2 replies
  • 0 kudos