2022-07-23 10:29 PM
Did the following
Create a very simple TouchGFX designer 1 screen with a button
generated code
closed TouchGFX designer
Open CubeIDE
Imported touchgfx project (ioc file)
Build CubeIDE project
Get the following build errors - Why doesn't the CubeIDE project build?
CubeIDE V1.10.1
TouchGFX V4.20.0
I have noticed in the forums that there seems to various ways of created TouchGFX and CubeIDE projects.
What is the ST preferred way of getting a project with TouchGFX into the CubeIDE environment, I am under the understanding that these environment are meant to work together. Is that the point of it all or.is my thinking here stupid.
11:02:35 **** Incremental Build of configuration Debug for project STM32H735G-DK ****
make -j16 all
arm-none-eabi-g++ "../TouchGFX/target/generated/OSWrappers.cpp" -mcpu=cortex-m7 -std=gnu++14 -g3 -DDEBUG -DUSE_HAL_DRIVER -DSTM32H735xx -c -I../Core/Inc -I../TouchGFX/App -I../TouchGFX/target/generated -I../TouchGFX/target -I../Drivers/STM32H7xx_HAL_Driver/Inc -I../Drivers/STM32H7xx_HAL_Driver/Inc/Legacy -I../Middlewares/Third_Party/FreeRTOS/Source/include -I../Middlewares/Third_Party/FreeRTOS/Source/CMSIS_RTOS_V2 -I../Middlewares/Third_Party/FreeRTOS/Source/portable/GCC/ARM_CM4F -I../Drivers/CMSIS/Device/ST/STM32H7xx/Include -I../Drivers/CMSIS/Include -IC:/TouchGFXProjects/Test12345/TouchGFX/generated/fonts/include -IC:/TouchGFXProjects/Test12345/TouchGFX/generated/gui_generated/include -IC:/TouchGFXProjects/Test12345/TouchGFX/generated/images/include -IC:/TouchGFXProjects/Test12345/TouchGFX/generated/texts/include -IC:/TouchGFXProjects/Test12345/TouchGFX/gui/include -O0 -ffunction-sections -fdata-sections -fno-exceptions -fno-rtti -fno-use-cxa-atexit -Wall -fstack-usage -MMD -MP -MF"TouchGFX/target/generated/OSWrappers.d" -MT"TouchGFX/target/generated/OSWrappers.o" --specs=nano.specs -mfpu=fpv5-d16 -mfloat-abi=hard -mthumb -o "TouchGFX/target/generated/OSWrappers.o"
arm-none-eabi-g++ "../TouchGFX/target/generated/STM32DMA.cpp" -mcpu=cortex-m7 -std=gnu++14 -g3 -DDEBUG -DUSE_HAL_DRIVER -DSTM32H735xx -c -I../Core/Inc -I../TouchGFX/App -I../TouchGFX/target/generated -I../TouchGFX/target -I../Drivers/STM32H7xx_HAL_Driver/Inc -I../Drivers/STM32H7xx_HAL_Driver/Inc/Legacy -I../Middlewares/Third_Party/FreeRTOS/Source/include -I../Middlewares/Third_Party/FreeRTOS/Source/CMSIS_RTOS_V2 -I../Middlewares/Third_Party/FreeRTOS/Source/portable/GCC/ARM_CM4F -I../Drivers/CMSIS/Device/ST/STM32H7xx/Include -I../Drivers/CMSIS/Include -IC:/TouchGFXProjects/Test12345/TouchGFX/generated/fonts/include -IC:/TouchGFXProjects/Test12345/TouchGFX/generated/gui_generated/include -IC:/TouchGFXProjects/Test12345/TouchGFX/generated/images/include -IC:/TouchGFXProjects/Test12345/TouchGFX/generated/texts/include -IC:/TouchGFXProjects/Test12345/TouchGFX/gui/include -O0 -ffunction-sections -fdata-sections -fno-exceptions -fno-rtti -fno-use-cxa-atexit -Wall -fstack-usage -MMD -MP -MF"TouchGFX/target/generated/STM32DMA.d" -MT"TouchGFX/target/generated/STM32DMA.o" --specs=nano.specs -mfpu=fpv5-d16 -mfloat-abi=hard -mthumb -o "TouchGFX/target/generated/STM32DMA.o"
../TouchGFX/target/generated/OSWrappers.cpp:20:10: fatal error: touchgfx/hal/HAL.hpp: No such file or directory
20 | #include <touchgfx/hal/HAL.hpp>
| ^~~~~~~~~~~~~~~~~~~~~~
compilation terminated.
make: *** [TouchGFX/target/generated/subdir.mk:28: TouchGFX/target/generated/OSWrappers.o] Error 1
make: *** Waiting for unfinished jobs....
In file included from ../TouchGFX/target/generated/STM32DMA.cpp:22:
../TouchGFX/target/generated/STM32DMA.hpp:22:10: fatal error: touchgfx/Bitmap.hpp: No such file or directory
22 | #include <touchgfx/Bitmap.hpp>
| ^~~~~~~~~~~~~~~~~~~~~
compilation terminated.
make: *** [TouchGFX/target/generated/subdir.mk:28: TouchGFX/target/generated/STM32DMA.o] Error 1
"make -j16 all" terminated with exit code 2. Build might be incomplete.
11:02:35 Build Failed. 5 errors, 0 warnings. (took 336ms)
2022-07-24 12:00 AM
You mix apples with berry
Imported touchgfx project (ioc file) ioc is MX project file.
For projects created in TGFX (not all) search IDE folder in and .project file. No ioc or other...
If you use KEIL search ...
Normal way to create custom TGFX isnt from TGFX, but new project in IDE or MX.
2022-07-24 1:50 AM
2022-07-24 1:59 AM
2022-07-24 2:14 AM
Yes you miss some steps.
Normal way is:
repeat 234 to working LCD
2022-07-25 12:57 AM
2022-07-25 4:17 AM
You skip Configure Software packand ...
2022-07-25 4:56 AM
OK, got it now.. thanks for your help :)
2022-07-25 10:55 PM