2021-07-24 12:48 AM
Hi,
when TouchGFX 4.17.0 is opened I'm getting an error stating no internet connectivity even though my laptop is connected to internet . also in the selection of boards I'm not getting any board option .
thanks and regards
sinduja
Solved! Go to Solution.
2021-07-26 2:11 AM
2021-07-24 10:08 PM
I have the same issue after updating from previous version v4.16.
Thanks,
VBK
2021-07-25 3:54 AM
i also have same problem..
my connection internet no have problem.. no use proxy.. and i think good connection..
already instal and uninstal.. even redownload the software on website.. but still same..
try instal version 4.17.0 and 4.16.1 same problem..anyone can help.. pls.
Thanks
Deni
2021-07-25 4:52 AM
me too...
2021-07-25 6:12 AM
I have the same issue, version 4.17 " You are not connected to internet and no demo or examples are available.
Anyway, the application is great! Thanks.
2021-07-25 8:36 AM
Hi,
I am also facing the same issue with all versions of TouchGFX. " You are not connected to internet and no demo or examples are available
2021-07-25 3:21 PM
Hi,
I also have same problem...
2021-07-25 3:33 PM
Hi,
I am having the same problems. No Internet connection, no demos, no examples, no boards to select...
Due to other problems I also just set up a completely new Windows system and newly installed all the latest STM Software with default settings. Still doesnt work...
2021-07-26 2:11 AM
Solved.
Guess the server was just down...
2021-09-13 4:45 AM
Hi,
I have the same problem with 4.17.0:
"No Internet connection"
Is the server down again?
Or could it be a problem with internet settings?
How can a proxy be configured in TouchGFX designer?
Thanks.