cancel
Showing results for 
Search instead for 
Did you mean: 

Need help configuring VL53L8 firmware

ay0and0
Visitor

Hello,

I’m working on a project where I have a Nucleo F401RE connected to a 53L8A1 expansion board. I’m able to get the histogram plot with the ToF sensor on the expansion board but am wondering if I will still be able to get it if I use an external trigger with a VL53L8 ToF sensor attached to the expansion board. If anyone knows if this is possible or has done it before, input would be greatly appreciated.
P.S. I am also using STM’s custom project, CUSTOM/VL53L8CX_SimpleRanging and I am using the histogram functionality with Example_12_cnh_data.c from their VL53LMZ_ULD folder.

Thank you!

0 REPLIES 0