cancel
Showing results for 
Search instead for 
Did you mean: 

Take data from one screen to another

BADA
Associate II

Hello everyone, I hope you can help me!!!

I'm at the beginning of programming in C++, and I'm having difficulty taking a variable from my main.c file to my screen created in touch gfx.

This error appears, where it apparently does not find the variable declaration.

 

Run Simulator
Generate
Done
Generate Assets
make -f simulator/gcc/Makefile assets -j8
Reading ./application.config
Reading ./target.config
Done
Post Generate
touchgfx update_project --project-file=simulator/msvs/Application.vcxproj
Done
Post Generate Target
touchgfx update_project
.cproject file: ../STM32CubeIDE/.cproject
Writing STM32CubeIDE project file: ../STM32CubeIDE/.project
Writing STM32CubeIDE project file: ../STM32CubeIDE/.cproject
Done
Compile
make -f simulator/gcc/Makefile -j8
Reading ./application.config
Reading ./target.config
Linking build/bin/simulator.exe
build/MINGW32_NT-6.2/gui/src/monitor_screen/MonitorView.o: In function `ZN11MonitorView15handleTickEventEv':
C:\TouchGFXProjects\MyApplication_2\TouchGFX/gui/src/monitor_screen/MonitorView.cpp:22: undefined reference to `dado'
collect2.exe: error: ld returned 1 exit status
generated/simulator/gcc/Makefile:160: recipe for target 'build/bin/simulator.exe' failed
make[2]: *** [build/bin/simulator.exe] Error 1
generated/simulator/gcc/Makefile:155: recipe for target 'generate_assets' failed
make[1]: *** [generate_assets] Error 2
simulator/gcc/Makefile:32: recipe for target 'all' failed
make: *** [all] Error 2
Failed


main c loop.png

 

 

 

main c.png

 

 

 

 

tela 1.png

 

I followed what the course instructor said, but apparently it doesn't work.

1 ACCEPTED SOLUTION

Accepted Solutions
Karl Yamashita
Principal

Looks like you're trying to take a short cut and not using MVP approach.

See this video tutorial on how to pass a variable, in this case an ADC value, from main to the Presenter

https://youtu.be/EbWOv_0Lp-U?si=s2OKKDyJN6vpb-3a

 

Don't worry, I won't byte.
TimerCallback tutorial! | UART and DMA Idle tutorial!

If you find my solution useful, please click the Accept as Solution so others see the solution.

View solution in original post

7 REPLIES 7
Kenwang
Associate III

I am not sure the value "dado" is in other .c file (ex : in main.c)

If yes, you can try modify line 18 to "extern int dado;"

 

Kenwang_0-1725437127950.png

 

mÆŽALLEm
ST Employee

Hello @BADA 

Next time, please paste your code using </> button instead sharing screenshots. Please refer to our recommendation here on how to post a thread in this community.

Thank you for your understanding.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

Hi, I removed the "C" and recompiled, but the same error appeared, I'm trying to backend an analog reading in main.c to the screen, I'm going to send the more simplified file of the project.

 

 

Karl Yamashita
Principal

Looks like you're trying to take a short cut and not using MVP approach.

See this video tutorial on how to pass a variable, in this case an ADC value, from main to the Presenter

https://youtu.be/EbWOv_0Lp-U?si=s2OKKDyJN6vpb-3a

 

Don't worry, I won't byte.
TimerCallback tutorial! | UART and DMA Idle tutorial!

If you find my solution useful, please click the Accept as Solution so others see the solution.

I can build your project in STM32CubeIDE 1.16.0 with touchGFX 4.24.0. Did you try to reinstall them ?

 

1.png

GaetanGodart
ST Employee

Hello @BADA  and welcome to the community! :smiling_face_with_smiling_eyes:

 

As other said, you can properly format your code (and log text) by using the </> button :

GaetanGodart_0-1725524788722.png

 

Regarding your question, since you created your variable from a TouchGFX file, you should include this file in your main.c.

Other than that, it is recommended to use the MVP design pattern to send or receive data from to GUI (TouchGFX) to the rest of the application (main.c and others). You can read more here : model-view-presenter-design-pattern 
Here is a video tutorial to send data from a screen to the main.c : Touch GFX #8. Send Data from UI to MCU || UART 

 

I hope this helps.
Once you solve your problem, I invite you to select the most helpful comment as "best answer".

 

Regards,

 

PS: If you want to properly display your code and log text using the </> button, you can do it by editing your message like so :

GaetanGodart_1-1725525093901.png

 

Gaetan Godart
Software engineer at ST (TouchGFX)

Really, I was doing the wrong process, thank you for the help and reference!!