2019-03-01 4:16 AM
Is there anywhere an Application Template available for this platform with the RGB TFT screen ?
Or any informations on how to do it, as it was asked here :
Display is the same as on the F746G-Discovery so it should be easy to adapt template from the F7 board. But I'm not able to find the place where already available Application Templates are provided ? Is it possible to get the well-formed archive somewhere locally when connecting to the remote server ?
Ideally, this Application Template should generate an ioc file to STM32CubeMX, same as with the F7 board. With this file, we can then adapt the project to build with TrueStudio and/or SW4STM32 (done sucessfully on the F746 with some manual changes)
2019-05-28 10:48 PM
Hi Martin,
We load this project in TouchGFX designer 4.10.0. It shows errors when doing code generation. We compile this project. It shows some files is missing. Could you help ? Thanks.
2019-05-29 12:15 AM
The first screenshot definitely says that you have no generated files (by designer) to compile. They cannot be found. The second confirms that code generation failed. I may need to see your project.
2019-05-29 12:38 AM
2019-05-29 6:18 PM
Hi Martin,
You said that this project is based on not-yet-released version of TouchGFX. I guess that's why file is missing. Could we work around by just offering me the missed files ?
2019-06-01 9:51 PM
I am definitely Interested can you provide it to me?
2019-06-03 1:25 AM
Hi @MHo.15,
I'll try to look at your project to get a better overview.
/Martin
2019-06-03 1:26 AM
Please look further up this post for a project. It's mostly for inspiration on initializing the LCD since the project is based on a version that isn't released yet. But take a look and let me know!
/Martin