2021-05-18 10:29 AM
Hi
I have two screens A and B.
On A ButtonSTART (Toggle).
On B ButtonSTOP (Toggle).
ButtonSTART is to change to screen B and turn on the counter.
ButtonSTOP is to change to screen A and stop the counter.
After changing screen A to B, ButtonSTART should be 0.
After changing screen B to A, ButtonSTOP should be 0.
How to set up GFX INTERACTION?
greetings
Andrzej
Solved! Go to Solution.
2021-05-21 6:10 AM
Not sure I get what you are trying to do. but you could set the "buttons" to 0 when you start the animation from a screen to another. You could do it through TouchGFX Designer in the Interactions tab by using the trigger "Screen Transition begins".
/Romain
2021-05-18 11:49 PM
Hi,
You could set the counter to 0 in the <nameOfScreen>View.cpp in the <nameOfScreen>::setupScreen function.
/Romain
2021-05-19 2:20 AM
Hi
I am not talking about the operation on the counter but about setting the buttons to 0 after changing the screen.
greetings
Andrzej
2021-05-19 7:09 AM
What do you mean by settings the buttons to 0 if it is not the counter ?
2021-05-19 8:41 AM
2021-05-21 6:10 AM
Not sure I get what you are trying to do. but you could set the "buttons" to 0 when you start the animation from a screen to another. You could do it through TouchGFX Designer in the Interactions tab by using the trigger "Screen Transition begins".
/Romain
2021-05-22 8:25 AM
Hi
I wrote a test program:
1.Press START
1.1 send button state to main.c
1.2 change screen
1.3 start htm3
2.Press STOP
2.1 sending button state to main.c
2.2 screen change 2.3 stop htm3
2.4 I set start = 0 in main.c
2.5 I set the counted pulses total_current = 0 in main.c
3.Press START I want him to change screen and count again.
How to do it?
Andrzej