2021-04-28 10:32 AM
Hi
I have a counter in main.c. I have two screens A and B. The meter reading is sent to screen B and displayed. When the counter reaches 0 I want screen B to switch to A. How to set it up in GFX? greetings
Andrzej
Solved! Go to Solution.
2021-05-05 6:00 AM
Are you sure the if(!min_current && !sec_current) condition is ever met ? The application().gotoScreenSetScreenNoTransition() function works.
/Romain
2021-05-05 6:48 AM
I checked the function works when there is no condition. In Live Expressions, sec_current and min_current change. I have yet to analyze.
2021-05-06 10:44 AM
Thank you for your help.
sec_current and min_current are in BCD so they were never 0.
I did this by sending a screen change request from main.c. It works.
I used:
application (). gotoScreenSetScreenNoTransition ();
Andrzej
2021-05-07 1:27 AM
Good to hear it works now :thumbs_up:
/Romain
2021-05-07 4:40 AM
What is the difference between the Click, Touch, Toggle buttons?
Andrzej