cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeIDE

AD�?b
Senior

I installed CubeIDE 1.2.0. There is no GRAPHICS graphics in Midleware. Why? In version 1.1.0 it was.

4 REPLIES 4
scottSD
Lead

See this thread: https://community.st.com/s/question/0D50X0000BwjU6pSQE/official-release-xcubetouchgfx-v4130

It is located under "Additional Software", but a few things have to be done to install it and activate it, which can be seen at this link:

https://touchgfx.zendesk.com/hc/en-us/articles/360011039799-Installing-TouchGFX

Thank you for the information. I returned to the previous version of STM32CubeIDE, i.e. to 1.1.0, and no additional treatments are needed there.

The links I gave you are specific to STM32CubeIDE 1.2.0 and TouchGFX 4.13.0 as well as CubeMX 5.5.0 (which is included with STMCubeIDE 1.2.0).

For now I will stay with version 1.1.0. I tried after installing touchGFX from the link but something went wrong. I will wait for it to be corrected. What facilities are in version 1.2.0?