2019-06-08 7:27 AM
Hi
I have followed this guide for the F7 to help setup an equivalent environment for the 32F469IDISCOVERY
https://www.youtube.com/watch?v=VOs2LYO7wSA
However I don't know which pin to select for the LCD reset and which protocol option to use:
Can anyone please advice?
Thanks
Robin
2019-06-09 8:48 AM
hi the 32F469IDISCOVERY use serial dsi host lcd
and i think the reset pin is j15
(the parallel options is usually for rgb screens )
2019-06-09 1:17 PM
Hi, Thanks for the advice the only pins available in the IDE for the LCD reset are:
PB2, PD4, PD5, PE2, PE3, PG6, PH7, PK3, PB0, PA3
Which of these if any map to J15?
2019-06-10 12:33 AM
sorry I got confused between the 32F469IDISCOVERY to 32F769IDISCOVERY in the f7 its j15.
and it seems that pin is PB0 because all the others are audio,leds,etc ..
good luck
2019-06-10 3:07 AM
Following the help so far I have set the display connection protocol to serial and assigned PB0 as the reset pin. I have been able to compile and build an image. I have loaded the image on the board using STM-LINK all good so far. When the debugger takes over the four LEDS light but the display is blank. Now I've placed a break point in the TouchGfx code on the Screen1ViewBase::Screen1ViewBase() constructor but the breakpoint is not being triggered.
My question is how does the TouchGfx code get called from main?
2019-06-10 3:08 AM
Following the help so far I have set the display connection protocol to serial and assigned PB0 as the reset pin. I have been able to compile and build an image. I have loaded the image on the board using STM-LINK all good so far. When the debugger takes over the four LEDS light but the display is blank. Now I've placed a break point in the TouchGfx code on the Screen1ViewBase::Screen1ViewBase() constructor but the breakpoint is not being triggered.
My question is how does the TouchGfx code get called from main?
2019-06-20 4:05 AM
This might be useful for others I have been able to put together a working CubeIDE STM32F469I-DISCO LCD and touch solution. Had to modify quite alot of the hal auto generated code.
https://github.com/Scubaboy/SMT32F7LCDDisco/tree/master/STMF4DISCOCubeIDE
2019-07-01 11:41 PM
I got Error How can i resolve it
../Src/OTM8009TouchController.cpp: In member function 'virtual void OTM8009TouchController::init()':
../Src/OTM8009TouchController.cpp:19:5: error: 'BSP_TS_Init' was not declared in this scope
BSP_TS_Init(LCD_GetXSize(), LCD_GetYSize());
^~~~~~~~~~~
../Src/OTM8009TouchController.cpp: In member function 'virtual bool OTM8009TouchController::sampleTouch(int32_t&, int32_t&)':
../Src/OTM8009TouchController.cpp:27:5: error: 'TS_StateTypeDef' was not declared in this scope
TS_StateTypeDef state;
^~~~~~~~~~~~~~~
../Src/OTM8009TouchController.cpp:28:24: error: 'state' was not declared in this scope
BSP_TS_GetState(&state);
^~~~~
../Src/OTM8009TouchController.cpp:28:24: note: suggested alternative: 'static'
BSP_TS_GetState(&state);
^~~~~
static
../Src/OTM8009TouchController.cpp:28:7: error: 'BSP_TS_GetState' was not declared in this scope
BSP_TS_GetState(&state);
^~~~~~~~~~~~~~~
make: *** [Src/subdir.mk:91: Src/OTM8009TouchController.o] Error 1
make: *** Waiting for unfinished jobs....
"make -j4 all" terminated with exit code 2. Build might be incomplete.
11:30:54 Build Failed. 6 errors, 1 warnings. (took 4s.613ms)
2019-07-01 11:55 PM
Couple of things to check first does your project contain the following source items.
Secondly I noticed your make command was 'make -j4 all' I'm using 'make -j12 all' also what version of make are you using?
2019-07-02 12:09 AM
I am Using
STM32CubeIDE
Version: 1.0.1
Build: 3139_20190612-1256 (UTC)
The Make is build in . How can i change that one.
My Files