2019-03-28 02:08 AM
Use cubemx to generate the project, then use the slider effect to switch screen and everything will run fine in the simulator.But I burned MDK to the hardware and didn't see the slider effect.Is there something wrong with the transplant?
Solved! Go to Solution.
2019-05-08 12:25 AM
I've modified the title of this post to be more concise, i hope that's okay with you: "Slide Transition animation effect does not show on target".
2019-05-08 12:58 AM
In 24-bit deep 800x480, use partition refresh.Why set the TE signal line scanline to 533 in LCD_ReqTear() instead of any other value?Can you explain the problem
2019-05-08 04:16 AM
Are fou facing an issue with this? Or just curious.
2019-05-08 06:09 PM
2019-05-10 12:45 AM
Do you have time to take a look? Thank you very much
2019-05-10 06:01 PM
When dual caching is enabled, Lowering the LTDC clock frequency solves this problem。