cancel
Showing results for 
Search instead for 
Did you mean: 

The CubeMX artificial limitations?

turboscrew
Senior III

Why are there such artificial limitations in CubeMX?

I tried to take FMC/NAND interface into use for a TFT LCD, so I don't need addresses or command/address latch strobes, but if, from the pin map, I change CLA into something else, the whole FMC/NAND disappears. The HW works fine without the mentioned pins - I've used the NAND-interface that way. It would just be nice to get the set-up also "documented" in the .ioc-file. I did it before by configuring the FMC/NAND and changing the address and latch pins in SW for other functions.

I couldn't use the NOR interface, because the display needed longer hold time than NOR could give.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0