cancel
Showing results for 
Search instead for 
Did you mean: 

Slide Transition animation effect does not show on target

lxw
Senior

Use cubemx to generate the project, then use the slider effect to switch screen and everything will run fine in the simulator.But I burned MDK to the hardware and didn't see the slider effect.Is there something wrong with the transplant?

15 REPLIES 15

I've modified the title of this post to be more concise, i hope that's okay with you: "Slide Transition animation effect does not show on target".

In 24-bit deep 800x480, use partition refresh.Why set the TE signal line scanline to 533 in LCD_ReqTear() instead of any other value?Can you explain the problem

Are fou facing an issue with this? Or just curious.

Yeah, curious why 533.

Another problem encountered: when I change the bottom layer to 24Bpp,800x480 is divided into two regions, 400x480 refresh, single buffering is OK.When dual caching is enabled, a short splash screen appears when the interface is switched on.

Do you have time to take a look? Thank you very much:loudly_crying_face:

When dual caching is enabled, Lowering the LTDC clock frequency solves this problem。:face_with_tears_of_joy: