2024-09-23 4:54 AM
Hi,
I have a custom board with STM32H743 and working on a project by TouchGFX 4.24. When the device power on or reset, some times I have a mixed image including numbers, pictures and ..., which I attached the image... and some times every thing is Ok after reset or power on. I have another project by TouchGFX on this board, which it always works fine.
Please help me with this, thanks.
2024-09-23 7:04 AM
I should add, the main difference between program with distorted program and the correct one is: distorted program GUI is imported from old version of it from TouchGFX Designer... Is there any problem with this?
BR
2024-09-23 7:11 AM
@MHaji.1 wrote:
Please post the corresponding image of what the screen should look like.
Note that you can paste the image into the post - where we can see it - rather than attaching it (where we can't).
2024-09-23 7:26 AM
Hi Andrew,
Thank you for reply.
As you see in the picture, The numbers are readable and the picture is correct, but in last one all screen is distorted.
Thanks
2024-09-23 7:32 AM - edited 2024-09-23 7:32 AM
Could this be uninitialised data?
ie, in your first case, the values are "junk", and this corrupts the display ?
PS:
especially if the data is passed via pointers, and it's the pointers that are uninitialised
2024-09-23 7:38 AM
No, The corrupted one is installed on a mold machine and the numbers are related to device, Here is a picture with the same as last pic which I sent:
As you see, There are some weird lines and numbers are corrupted, picture has lot of noise and...
2024-09-23 8:12 AM
Hello,
You said:
@MHaji.1 wrote:
I have another project by TouchGFX on this board, which it always works fine.
Is it working on the same MCU part number i.e. STM32H743?
2024-09-23 8:27 AM
Hello,
Thanks for reply,
Yes, The part numbers are the same.
2024-09-23 8:30 AM
@MHaji.1 wrote:
Yes, The part numbers are the same.
So make a diff with the projects!
2024-09-23 8:48 AM
I have 3 different project which are almost have same content, but with a different user (different devices).. I have no problem with 2 of them, but the one which we speaking about has this problem, after power off and power on, the problem will solved, but in another power on, I face this corrupted state..
PS:
The GUI is imported from its old version in corrupted image device...