2020-03-13 04:57 PM
I am trying to make a graph with touchgfx4.13 on stm32f746g_disco .
I am using CubeIDE ver 1.3.0
I tried to use Canvas Widget and used the sample codes on touchgfx zendesk site .
If I can draw even a line in a box I will be able to make the graph.
I hope Martin himself can make Kindly a video about it ,
2020-03-17 06:50 AM
I made it work on my STM32F429 VGA project.
There is graph widget on GitHub TouchGFX Open Repository:
https://github.com/touchgfx/touchgfx-open-repository/tree/master/widgets/Graph
Download it and put in the paths like in the original project.
The picture shows it in my STM32CubeIDE.
Then you only need to edit your ScreenXXXView.hpp:
#ifndef SCREENAVIEW_HPP
#define SCREENAVIEW_HPP
#include <gui_generated/screena_screen/screenAViewBase.hpp>
#include <gui/screena_screen/screenAPresenter.hpp>
#include <gui/common/Graph.hpp>
class screenAView : public screenAViewBase
{
public:
screenAView();
virtual ~screenAView() {}
virtual void setupScreen();
virtual void tearDownScreen();
virtual void handleTickEvent();
protected:
int tickCounter;
int graph_YVal
Graph graph;
};
#endif // SCREENAVIEW_HPP
And your ScreenXXXView.cpp:
#include <gui/screena_screen/screenAView.hpp>
screenAView::screenAView()
{
}
void screenAView::setupScreen()
{
screenAViewBase::setupScreen();
// Place the graph on the screen
graph.setXY(20, 20);
// Set the outer dimensions and color of the graph
graph.setup(400, 200, Color::getColorFrom24BitRGB(0xFF, 0xFF, 0x00));
// Set the range for the x and y axis of the graph. That is
// the max and min x/y value that can be displayed inside the
// dimension of the graph.
graph.setRange(0, 400, 0, 200);
// Set the line width in pixels
graph.setLineWidth(1);
add(graph);
}
void screenAView::tearDownScreen()
{
screenAViewBase::tearDownScreen();
}
void screenAView::handleTickEvent(){
// Number of ticks between inserting a point in the graph
int interval = 1;
if (tickCounter % interval == 0)
{
graph.addValue(tickCounter / interval, graph_YVal);
graph_YVal+=5;
}
if ((tickCounter % (10 * interval)) == 0)
{
graph_YVal = 0;
}
tickCounter++;
if (tickCounter == 400 * interval)
{
graph.clear();
graph.invalidate();
tickCounter = 0;
graph_YVal = 0;
}
}
More you can do with graph you can find in TemplateView.cpp in the repository (link above).
My "code" draws a saw-like curve.
Jiri K.
2020-03-20 05:36 PM
Hi Jiri
Thanks so much I earlier saw your file and learned so much from that .
actually you used two line segment for each segment , it was so genius . I didn't use your Abstarct Graph , and directly used CanvasWidget but the same Idea as yours and finally I could make the graph as attached . I have two question
1- is there any straight way to draw a set of open lines , simply without having to render those as a closed shape .
2- I have to put TickCounter around 50 to work otherwise it can not invalidate completely , it draw just a random part of the container not all of that .
Any way I like to thank you again for your contribution .
Morteza
2020-03-25 10:57 AM
Nonono I did not write the Github code, I only used it an shared 🙂
I was also searching for some CanvasWidget example...