2022-06-29 09:19 AM
Hi,
I have integrated with lwIP and freeRTOS a VNC server on a STM32H757-EVAL.
A VNC client works fine and I can see on it the first frame buffer drawn by the application; according to the VNC standard, the server should send a "new tile" (a square of pixel) to re-draw the frame buffer changed (if something happens and change it - i.e. slider, button clicked, etc..).
Is there any function or method to understand which pixel (or pixelS) has changed (in term of X and Y coordinates) from the previous frame buffer?
In this way, I can recreate a new tile and send it to the VNC client without re-send every time the whole frame buffer using less bandwidth.
Thanks for your help.
Regards.
Solved! Go to Solution.
2022-06-30 07:13 AM
Try breakpoint and check rect
/**
* This function is called whenever the framework has performed a partial draw.
*
* @param rect The area of the screen that has been drawn, expressed in absolute coordinates.
*
* @see flushFrameBuffer().
*/
void TouchGFXHAL::flushFrameBuffer(const touchgfx::Rect& rect)
{
// Calling parent implementation of flushFrameBuffer(const touchgfx::Rect& rect).
//
// To overwrite the generated implementation, omit call to parent function
// and implemented needed functionality here.
// Please note, HAL::flushFrameBuffer(const touchgfx::Rect& rect) must
// be called to notify the touchgfx framework that flush has been performed.
TouchGFXGeneratedHAL::flushFrameBuffer(rect);
}
2022-06-29 10:07 AM
In partial framebuffer mode you can simple handle this in handle rectangle target implementation.
For full single or double you can too use target parts of code ...
2022-06-30 03:37 AM
What VNC server do you use?
2022-06-30 03:45 AM
Hi,
in my case I'm using full single buffer for my display.
Do you think that the API for partial frame buffer continue to work even if I set it as REFRESH_STRATEGY_DEFAULT? Because I use a LTDC-DSI display in video mode and I don't need to re-write touchgfxDisplayDriverTransmitActive or touchgfxDisplayDriverTransmitBlock.
2022-06-30 03:48 AM
I use VNC server from ecos operating System; on the internet you can find VNC server source code and adapt it to FreeRTOS and LWIP.
2022-06-30 03:54 AM
I am doing actually the same thing (also ecos). Not using any of their drawing ot text functions (thanks to TouchGFX), but you just step ahead of me 🙂 I was thinking to extend Invalidate() function because it should contain coordinates of area was drawn, but I not realized this idea yet.
2022-06-30 04:01 AM
Now I'm trying to understand if I can use API for partial frame buffer strategy (as suggest by @MM..1 . After that I can check Invalidate function. Let me know if you can try it before I do.
2022-06-30 07:13 AM
Try breakpoint and check rect
/**
* This function is called whenever the framework has performed a partial draw.
*
* @param rect The area of the screen that has been drawn, expressed in absolute coordinates.
*
* @see flushFrameBuffer().
*/
void TouchGFXHAL::flushFrameBuffer(const touchgfx::Rect& rect)
{
// Calling parent implementation of flushFrameBuffer(const touchgfx::Rect& rect).
//
// To overwrite the generated implementation, omit call to parent function
// and implemented needed functionality here.
// Please note, HAL::flushFrameBuffer(const touchgfx::Rect& rect) must
// be called to notify the touchgfx framework that flush has been performed.
TouchGFXGeneratedHAL::flushFrameBuffer(rect);
}
2022-06-30 07:17 AM
Hi @MM..1 ,
I was exactly trying this and it works.
I report below the modified code.
void TouchGFXHAL::flushFrameBuffer(const touchgfx::Rect& rect)
{
// Calling parent implementation of flushFrameBuffer(const touchgfx::Rect& rect).
//
// To overwrite the generated implementation, omit call to parent function
// and implemented needed functionality here.
// Please note, HAL::flushFrameBuffer(const touchgfx::Rect& rect) must
// be called to notify the touchgfx framework that flush has been performed.
/* USER CODE BEGIN flushFrameBuffer step 1 */
TouchGFXGeneratedHAL::flushFrameBuffer(rect);
extern volatile int tile_updated[NUM_TILES_Y_AXIS][NUM_TILES_X_AXIS];
extern SemaphoreHandle_t s_xMutexClientLock;
extern SemaphoreHandle_t s_xSemphClientWait;
extern volatile int update_req;
uint16_t i,j;
printf("RECT: x=%d, y=%d, width=%d, height=%d\r\n",
rect.x, rect.y, rect.width, rect.height);
if(s_xSemphClientWait != NULL && s_xMutexClientLock != NULL)
{
/* Non-incremental mode - mark the squares that need to be updated */
for (i = (rect.x)/TILE_SIZE;
i <= (rect.x + rect.width)/TILE_SIZE;
i++)
{
for (j = (rect.y)/TILE_SIZE;
j <= (rect.y + rect.height)/TILE_SIZE;
j++)
{
tile_updated[j][i] = 1;
}
}
xSemaphoreTake(s_xMutexClientLock, portMAX_DELAY);
update_req = 1;
printf("signal da flushFrameBuffer\r\n");
xSemaphoreGive(s_xMutexClientLock);
xSemaphoreGive(s_xSemphClientWait);
}
/* USER CODE END flushFrameBuffer step 1 */
}
2022-08-31 01:23 AM
Hi @Danix2k and @ktrofimo,
did you managed to sucessfuly port ecos VNC to freertos+lwip+touchgfx ? Are you willing to share project or source code for it ?
Best regards