2020-12-22 6:24 AM
I have a problem that I cannot include C code in C++ and the opposite. Different sites suggest to solve this problem by including the header file of C in the header file of C++ (Model.hpp) like:
#ifdef __cplusplus
extern "C"{
#endif
#include "coreTransferBufferAPI.h"
#ifdef __cplusplus
}
#endif
In the code file Model.cpp, I try to use a function called (CB_Display_GetValues(&values) from this header.
CB_DisplayValues_t is also defined in this header, but doesn't show any errors.
float Model::getTempValue()
{
CB_DisplayValues_t values;
if(CB_Display_GetValues(&values)==REPORT_OK)
{
return values.cellTemperature;
}
return NULL;
}
The call of the function (CB_Display_GetValues(&values)) gives an undefined reference error:
/../TouchGFX/gui/src/model/Model.cpp:32: undefined reference to `CB_Display_GetValues'
Do you have a solution for this problem or do you know how to solve it? How would including a C++ code in C work (opposite way)?
Thank you very much and a festive holiday, K.Frey1
Solved! Go to Solution.
2020-12-22 6:48 AM
Calling C code from C++ is easy. Ensure the function is declared prior to calling it (typically by including the appropriate header) and just call the function. Perhaps there is a typo or other mistake which is preventing this from working in your case.
Calling C++ code from C is more complicated. You need to ensure the functions have C linkage by enclosing them in extern "C" braces, and then you just call them.
2020-12-22 6:48 AM
Calling C code from C++ is easy. Ensure the function is declared prior to calling it (typically by including the appropriate header) and just call the function. Perhaps there is a typo or other mistake which is preventing this from working in your case.
Calling C++ code from C is more complicated. You need to ensure the functions have C linkage by enclosing them in extern "C" braces, and then you just call them.
2020-12-24 7:17 AM
Dear TDK, thank you for your reply.
As you can see, I did declare the c-type header-file prior to calling it and then called the function. I don't think it's a typo because I checked it several times and you can see the code above. What other mistake could it possibly be?
2020-12-24 8:34 AM
Where is CB_Display_GetValues defined (C or CPP file name, not header)? Is that file getting compiled? Examine the console log and show proof.
2020-12-26 11:21 AM
TDK, you were right "CB_Display_GetValues" a function in the c-headerfile was not properly declared. Thank you, and sorry for your trouble