2025-03-04 4:48 PM - edited 2025-03-04 4:50 PM
Hello ST Team,
I'm trying to bring up I3C using a NUCLEO-H563ZI with XNUCLEO-IKS4A1 to boards stress I3C, and I'm using AN5879, which was thought for NUCLEO-H503RB and X-NUCLEO-IKS01A3 boards.
Regardless of the above, I still believe we should be able to work with these boards as they are I3C compatible, and the XNUCLEO-IKS4A1 is marked as the new alternative for the X-NUCLEO-IKS01A3 board.
I'm following AN5879 to introduce myself to I3C (and the entire STM32CubeIDE ecosystem), and I have found issues adding the extra code stated on page 31 (software settings for dynamic addressing).
Where precisely should these lines be introduced? For the four code blocks, I can identify the second and the fourth ones belonging to the main.c file. What about the first and third blocks? For the first, it seems I should create a new header file stm32_i3c_desc_target1.h, but even when creating this file and adding a reference in main.h the compiler struggles to find "TargetDesc_Typedef". My best guess is to include the third block at the last part of the MX_I3C1_Init function described in main.c.
Returning to the fourth block:
void HAL_I3C_TgtReqDynamicAddrCallback(I3C_HandleTypeDef *hi3c, uint64_t targetPayload)
{
TargetDesc1.TARGET_BCR_DCR_PID = targetPayload;
HAL_I3C_Ctrl_SetDynAddr(hi3c, TargetDesc1.DYNAMIC_ADDR);
}
void HAL_I3C_CtrlDAACpltCallback(I3C_HandleTypeDef *hi3c)
{
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_5, GPIO_PIN_SET);
}
Could you please give me a hand checking if this GPIO reference to pin 5 and GPIOA is still valid for the NUCLEO-H563ZI board?
Thank you, D.
Solved! Go to Solution.
2025-03-05 1:32 PM
I found out some answers after opening an example demo using I3C (I3C_Controller_Direct_Command_DMA).
The first block:
#define TARGET1_DYN_ADDR 0x32
/********************/
/* Target Descriptor */
/********************/
TargetDesc_TypeDef TargetDesc1 =
{
"TARGET_ID1",
DEVICE_ID1,
0x0000000000000000,
0x00,
TARGET1_DYN_ADDR,
};should go in a new header file (named here desc_target1.h as in the example) and referenced in the main.c after including main.h:
#include "main.h"
#include "desc_target1.h"The typedef description should be added in main.h:
/* USER CODE BEGIN ET */
/* Target descriptor */
typedef struct {
char * TARGET_NAME; /*!< Marketing Target reference */
uint32_t TARGET_ID; /*!< Target Identifier on the Bus */
uint64_t TARGET_BCR_DCR_PID; /*!< Concatenation value of PID, BCR and DCR of the target */
uint8_t STATIC_ADDR; /*!< Static Address of the target, value found in the datasheet of the device */
uint8_t DYNAMIC_ADDR; /*!< Dynamic Address of the target preset by software/application */
} TargetDesc_TypeDef;
/* USER CODE END ET */The device ID also needs to be defined in the main.h file:
/* USER CODE BEGIN Private defines */
/* Define Target Identifier */
#define DEVICE_ID1 0U
/* USER CODE END Private defines */The third block can go after I3C is initialized (MX_I3C1_Init() in main.c):
/* USER CODE BEGIN 2 */
/* Assign dynamic address processus */
if (HAL_I3C_Ctrl_DynAddrAssign_IT(&hi3c1, I3C_ONLY_ENTDAA) != HAL_OK)
{
/* Error_Handler() function is called when error occurs. */
Error_Handler();
}
/* USER CODE END 2 */Regarding the last doubt from the fourth block,
/* USER CODE BEGIN 4 */
void HAL_I3C_TgtReqDynamicAddrCallback(I3C_HandleTypeDef *hi3c, uint64_t targetPayload)
{
TargetDesc1.TARGET_BCR_DCR_PID = targetPayload;
HAL_I3C_Ctrl_SetDynAddr(hi3c, TargetDesc1.DYNAMIC_ADDR);
}
void HAL_I3C_CtrlDAACpltCallback(I3C_HandleTypeDef *hi3c)
{
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_5, GPIO_PIN_SET);
}
/* USER CODE END 4 */I can now tell (please correct if I'm wrong) HAL_I3C_CtrlDAACpltCallback is called as an acknowledgement of a successful dynamic address assignment. So the way to tell the user of this can be, for example, a LED turn on:
void HAL_I3C_CtrlDAACpltCallback(I3C_HandleTypeDef *hi3c)
{
BSP_LED_On(LED_GREEN);
}After these additions, I can compile, program the board and see SCL/SDA transactions.
2025-03-05 1:32 PM
I found out some answers after opening an example demo using I3C (I3C_Controller_Direct_Command_DMA).
The first block:
#define TARGET1_DYN_ADDR 0x32
/********************/
/* Target Descriptor */
/********************/
TargetDesc_TypeDef TargetDesc1 =
{
"TARGET_ID1",
DEVICE_ID1,
0x0000000000000000,
0x00,
TARGET1_DYN_ADDR,
};should go in a new header file (named here desc_target1.h as in the example) and referenced in the main.c after including main.h:
#include "main.h"
#include "desc_target1.h"The typedef description should be added in main.h:
/* USER CODE BEGIN ET */
/* Target descriptor */
typedef struct {
char * TARGET_NAME; /*!< Marketing Target reference */
uint32_t TARGET_ID; /*!< Target Identifier on the Bus */
uint64_t TARGET_BCR_DCR_PID; /*!< Concatenation value of PID, BCR and DCR of the target */
uint8_t STATIC_ADDR; /*!< Static Address of the target, value found in the datasheet of the device */
uint8_t DYNAMIC_ADDR; /*!< Dynamic Address of the target preset by software/application */
} TargetDesc_TypeDef;
/* USER CODE END ET */The device ID also needs to be defined in the main.h file:
/* USER CODE BEGIN Private defines */
/* Define Target Identifier */
#define DEVICE_ID1 0U
/* USER CODE END Private defines */The third block can go after I3C is initialized (MX_I3C1_Init() in main.c):
/* USER CODE BEGIN 2 */
/* Assign dynamic address processus */
if (HAL_I3C_Ctrl_DynAddrAssign_IT(&hi3c1, I3C_ONLY_ENTDAA) != HAL_OK)
{
/* Error_Handler() function is called when error occurs. */
Error_Handler();
}
/* USER CODE END 2 */Regarding the last doubt from the fourth block,
/* USER CODE BEGIN 4 */
void HAL_I3C_TgtReqDynamicAddrCallback(I3C_HandleTypeDef *hi3c, uint64_t targetPayload)
{
TargetDesc1.TARGET_BCR_DCR_PID = targetPayload;
HAL_I3C_Ctrl_SetDynAddr(hi3c, TargetDesc1.DYNAMIC_ADDR);
}
void HAL_I3C_CtrlDAACpltCallback(I3C_HandleTypeDef *hi3c)
{
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_5, GPIO_PIN_SET);
}
/* USER CODE END 4 */I can now tell (please correct if I'm wrong) HAL_I3C_CtrlDAACpltCallback is called as an acknowledgement of a successful dynamic address assignment. So the way to tell the user of this can be, for example, a LED turn on:
void HAL_I3C_CtrlDAACpltCallback(I3C_HandleTypeDef *hi3c)
{
BSP_LED_On(LED_GREEN);
}After these additions, I can compile, program the board and see SCL/SDA transactions.