cancel
Showing results for 
Search instead for 
Did you mean: 

How can I use Japanese?

Ebun.1
Senior

Thank you for helping.

How can I use English and Japanese?

Can you speak Japanese even if you run the simulator? The characters are garbled.

1 ACCEPTED SOLUTION

Accepted Solutions

Hi,

The issue you faced is due to the font you selected. You need to use a font that properly handles Japanese. I used for example IPA which is enclosed in the project attached.

/Romain

View solution in original post

6 REPLIES 6
Alexandre RENOUX
Principal

Hello Ebun.1,

Using Japanese and English should be pretty straight forward. Could you enclose your project so that I can have a quick look ?

/Alexandre

Ebun.1
Senior

Hi Alexandre RENOUX

Thank you for helping.

Attach the compressed file of the project.

( made by TouchGFX Ver4.16.1 )​

Thank you.

Hi,

The issue you faced is due to the font you selected. You need to use a font that properly handles Japanese. I used for example IPA which is enclosed in the project attached.

/Romain

Ebun.1
Senior

Hi Romain Dieleman

Thank you for helping.

Thank you for adding it to the project.

Where should I touch? I understood about.

I cried for "麦�?ら�?�一味" . (^_^)

Sorry, I don't think we understand. You wrote "where should I touch?". Is your problem fixed now?

�?��?ん�?分�?�り�?��?�ん。「�?��?��?�触り�?��?��?��?�?�書�??�?��?��?�。​今�?題�?��?��?��?��?��?�?

Embedded UI/UX Consulting: cadenza.design
Ebun.1
Senior

Hi Michael K

Thank you for helping.

I was able to understand where to modify the display in Japanese.

No problem.

Thank you very much.