Skip to main content
Visitor II
November 18, 2024
Question

Regarding SWD connection between STM32F411RE and ST-LINK/V2-ISOL

  • November 18, 2024
  • 1 reply
  • 877 views

After connecting to STM32F411RE for debugging using ST-LINK/V2-ISOL, I am trying to write a program using CUBEProgrammer, but the following error occurs. If anyone knows the cause, I would appreciate it if you could let me know.

Error: STM32 target not found! If your product has debug authentication built-in, please run discovery using debug authentication

 

[conditions]

・PC and ST-LINK/V2-ISOL: USB connection

・PC and STM32F411RE: USB connection

・STM32F411RE and ST-LINK/V2-ISOL

>CN2 jumper OFF

>JP1 jumper ON

>CN4:1 pin=CN6:4 pin

>CN4:2 pin=STLINK:9 pin

>CN4:3 pin=STLINK:12 pin

>CN4:4 pin=STLINK:7 pin

>CN4:5 pin=STLINK:15 pin

 

This post has been translated from Japanese to comply with the ST Community guidelines.

 

This topic has been closed for replies.

1 reply

ST Technical Moderator
November 18, 2024

Hello @oren and welcome to the Community;

Try following the steps on this article: How to solve debugger connection issues - STMicroelectronics Community

Did you make any modification on the board?

Maybe your target does not have power. Try set power on the VDD.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks