cancel
Showing results for 
Search instead for 
Did you mean: 

How can I make 90deg keyboard on 272x480 screen?

Ayagb.2239
Associate II

Hello,

I saw keyboard example but all example for 180deg display orientation. I am using 480x272 LCD but screen orientation is 90deg than ı have 272x480 screen. In examples keyboard is on 320x240. How can I use this examples or Any solution avaiable ?

Thanks.

Ahmet.

4 REPLIES 4
Alexandre RENOUX
Principal

Hello,

Are you saying that you are using a screen in a vertical manner ? In which case, you have to adapt the examples accordingly like changing size and position of widgets but the logic behind should stay the same.

/Alexandre

Ayagb.2239
Associate II

Hi dear Alexandre,

Yes right vertical. You mean adapt example ( I need to chande keyboard image size and I need to set keyboard button address and positions ?)

Thanks.

Hello,

Yes you need to change the layout of the keyboard so that it matches your screen. Refer to Keyboard.hpp and KeyboardLayout.hpp in the Keyboard example available on the Designer.

/Alexandre

Ayagb.2239
Associate II

Hi dear Alexandre,

Thank you.