cancel
Showing results for 
Search instead for 
Did you mean: 

Generate Code & Run Simulator Fail

Iris-DM
Associate III

I have come back to TouchGFXDesigner after not using it for about 6 months. I have updated to 4.26.0 and created a new blank project for the STM32H747I-DISCO board. When trying to generate code, I get the following error message:

Generate Code
Generate
Done
Generate Assets
make -f simulator/gcc/Makefile assets -j8
'M' is not recognized as an internal or external command,
operable program or batch file.
Failed
Failed

Looking through the Makefile, I can't see anywhere that this 'M' would be generated, and make isn't overridden in my environment variables.

13 REPLIES 13
mƎALLEm
ST Employee

Hello,

I've just created a blank TouchGFX project starting from STM32H747I-DISCO, generated the code and didn't face any issue (I'm using TouchGFX 4.26 + CubeMx 6.16). This is the log I had:

Generate Code
    Copy Framework
        Copying TouchGFX framework version 4.26.0 to C:\TouchGFXProjects\STM32H747I-DISCO\CM7\Middlewares\ST\touchgfx
        Done
    Generate
        Wrote config/gcc/app.mk
        Wrote config/msvs/Application.props
        Wrote generated/gui_generated/include/gui_generated/common/FrontendApplicationBase.hpp
        Wrote generated/gui_generated/include/gui_generated/common/FrontendHeapBase.hpp
        Wrote generated/gui_generated/include/gui_generated/common/SimConstants.hpp
        Wrote generated/gui_generated/include/gui_generated/screen1_screen/Screen1ViewBase.hpp
        Wrote generated/gui_generated/src/common/FrontendApplicationBase.cpp
        Wrote generated/gui_generated/src/screen1_screen/Screen1ViewBase.cpp
        Wrote generated/simulator/gcc/Makefile
        Wrote generated/simulator/include/simulator/mainBase.hpp
        Wrote generated/simulator/include/simulator/video/DirectFrameBufferVideoController.hpp
        Wrote generated/simulator/include/simulator/video/MJPEGDecoder.hpp
        Wrote generated/simulator/include/simulator/video/SoftwareMJPEGDecoder.hpp
        Wrote generated/simulator/msvs/touchgfx_prebuild.targets
        Wrote generated/simulator/msvs/touchgfx_sdl2.props
        Wrote generated/simulator/msvs/touchgfx.props
        Wrote generated/simulator/src/mainBase.cpp
        Wrote generated/simulator/src/video/SoftwareMJPEGDecoder.cpp
        Wrote generated/simulator/touchgfx.ico
        Wrote generated/simulator/touchgfx.rc
        Wrote generated/simulator/touchgfx.res
        Wrote generated/user.config
        Wrote gui/include/gui/common/FrontendApplication.hpp
        Wrote gui/include/gui/common/FrontendHeap.hpp
        Wrote gui/include/gui/model/Model.hpp
        Wrote gui/include/gui/model/ModelListener.hpp
        Wrote gui/include/gui/screen1_screen/Screen1Presenter.hpp
        Wrote gui/include/gui/screen1_screen/Screen1View.hpp
        Wrote gui/src/common/FrontendApplication.cpp
        Wrote gui/src/model/Model.cpp
        Wrote gui/src/screen1_screen/Screen1Presenter.cpp
        Wrote gui/src/screen1_screen/Screen1View.cpp
        Wrote simulator/gcc/Makefile
        Wrote simulator/main.cpp
        Wrote simulator/msvs/Application.sln
        Wrote simulator/msvs/Application.vcxproj
        Wrote simulator/msvs/Application.vcxproj.filters
        Wrote target.config
        Done
    Generate Assets
        make -f simulator/gcc/Makefile assets -j8
        Reading ./application.config
        Reading ./target.config
        Generating generated/images/include/BitmapDatabase.hpp
        Generating generated/images/include/images/BitmapDatabase.hpp
        Generating generated/images/src/BitmapDatabase.cpp
        Generating generated/images/include/images/SVGDatabase.hpp
        Generating generated/images/src/SVGDatabase.cpp
        Generating generated/videos/include/videos/VideoDatabase.hpp
        Cleaning generated files from generated/texts and generated/fonts.
        Generating generated/fonts/include/fonts/GeneratedFont.hpp
        Generating generated/fonts/src/GeneratedFont.cpp
        Generating generated/fonts/include/fonts/UnmappedDataFont.hpp
        Generating generated/fonts/src/UnmappedDataFont.cpp
        Generating generated/fonts/include/fonts/CachedFont.hpp
        Generating generated/fonts/src/CachedFont.cpp
        Generating generated/fonts/include/fonts/FontCache.hpp
        Generating generated/fonts/src/FontCache.cpp
        Generating generated/fonts/src/CompressedFontCache.cpp
        Generating generated/fonts/src/CompressedUnmappedFontCache.cpp
        Generating generated/fonts/include/fonts/CompressedFontCache.hpp
        Generating generated/fonts/include/fonts/CompressedUnmappedFontCache.hpp
        Generating generated/fonts/src/ApplicationFontProvider.cpp
        Generating generated/fonts/include/fonts/ApplicationFontProvider.hpp
        Generating generated/texts/include/texts/TextKeysAndLanguages.hpp
        Generating generated/texts/include/texts/TypedTextDatabase.hpp
        Generating generated/texts/src/TypedTextDatabase.cpp
        Generating generated/texts/src/Texts.cpp
        Generating generated/texts/src/LanguageGb.cpp
        Generating generated/fonts/src/Font_verdana_10_4bpp_0.cpp
        Generating generated/fonts/src/Table_verdana_10_4bpp.cpp
        Generating generated/fonts/src/Kerning_verdana_10_4bpp.cpp
        Generating generated/fonts/src/Font_verdana_20_4bpp_0.cpp
        Generating generated/fonts/src/Table_verdana_20_4bpp.cpp
        Generating generated/fonts/src/Kerning_verdana_20_4bpp.cpp
        Generating generated/fonts/src/Font_verdana_40_4bpp_0.cpp
        Generating generated/fonts/src/Table_verdana_40_4bpp.cpp
        Generating generated/fonts/src/Kerning_verdana_40_4bpp.cpp
        Generating generated/fonts/src/VectorFontRendererBuffers.cpp
        Done
    Post Generate
        touchgfx update_project --project-file=simulator/msvs/Application.vcxproj
        Done
    Post Generate Target
        touchgfx update_project
        .cproject file: ../../STM32CubeIDE/CM7/.cproject
        Writing STM32CubeIDE project file: ../../STM32CubeIDE/CM7/.project
        Writing STM32CubeIDE project file: ../../STM32CubeIDE/CM7/.cproject
        Done
    Done
To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
Iris-DM
Associate III

Ok so my issue is occurring during the Generate Assets step - specifically between the make command and reading application.config

 

Generate Assets
        make -f simulator/gcc/Makefile assets -j8
        Reading ./application.config

 I have to assume at some point, a path is being incorrectly parsed, or a command overwritten to give us a standalone M in whatever command environment TouchGFX is using to run the makefile/generation script. How can I narrow down where this is?

I'm not expert of TouchGFX but what CubeMx are you using? the latest version 6.16? 

If you have a doubt about the path try to change the path and try with a short path ..

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
Iris-DM
Associate III

I've shortened the path with a new project and still get the same error - using CubeMX 6.16

Generate Code
    Copy Framework
        Copying TouchGFX framework version 4.26.0 to H:\TouchGFX\Projects\MyApplication\CM7\Middlewares\ST\touchgfx
        Done
    Generate
        Wrote config/gcc/app.mk
        Wrote config/msvs/Application.props
        Wrote generated/gui_generated/include/gui_generated/common/FrontendApplicationBase.hpp
        Wrote generated/gui_generated/include/gui_generated/common/FrontendHeapBase.hpp
        Wrote generated/gui_generated/include/gui_generated/common/SimConstants.hpp
        Wrote generated/gui_generated/include/gui_generated/screen1_screen/Screen1ViewBase.hpp
        Wrote generated/gui_generated/src/common/FrontendApplicationBase.cpp
        Wrote generated/gui_generated/src/screen1_screen/Screen1ViewBase.cpp
        Wrote generated/simulator/gcc/Makefile
        Wrote generated/simulator/include/simulator/mainBase.hpp
        Wrote generated/simulator/include/simulator/video/DirectFrameBufferVideoController.hpp
        Wrote generated/simulator/include/simulator/video/MJPEGDecoder.hpp
        Wrote generated/simulator/include/simulator/video/SoftwareMJPEGDecoder.hpp
        Wrote generated/simulator/msvs/touchgfx_prebuild.targets
        Wrote generated/simulator/msvs/touchgfx_sdl2.props
        Wrote generated/simulator/msvs/touchgfx.props
        Wrote generated/simulator/src/mainBase.cpp
        Wrote generated/simulator/src/video/SoftwareMJPEGDecoder.cpp
        Wrote generated/simulator/touchgfx.ico
        Wrote generated/simulator/touchgfx.rc
        Wrote generated/simulator/touchgfx.res
        Wrote generated/user.config
        Wrote gui/include/gui/common/FrontendApplication.hpp
        Wrote gui/include/gui/common/FrontendHeap.hpp
        Wrote gui/include/gui/model/Model.hpp
        Wrote gui/include/gui/model/ModelListener.hpp
        Wrote gui/include/gui/screen1_screen/Screen1Presenter.hpp
        Wrote gui/include/gui/screen1_screen/Screen1View.hpp
        Wrote gui/src/common/FrontendApplication.cpp
        Wrote gui/src/model/Model.cpp
        Wrote gui/src/screen1_screen/Screen1Presenter.cpp
        Wrote gui/src/screen1_screen/Screen1View.cpp
        Wrote simulator/gcc/Makefile
        Wrote simulator/main.cpp
        Wrote simulator/msvs/Application.sln
        Wrote simulator/msvs/Application.vcxproj
        Wrote simulator/msvs/Application.vcxproj.filters
        Wrote target.config
        Done
    Generate Assets
        make -f simulator/gcc/Makefile assets -j8
        'M' is not recognized as an internal or external command,
        operable program or batch file.
        Failed
    Failed

 

Hello,

Is that possible to zip and attach that project so I can test it and if I could reproduce the bahavior?

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
Iris-DM
Associate III

No problem - attached

Meanwhile,  the upload is stuck in (Virus scan in progress ...) :\ ! The issue is seen yesterday!

Refer to this thread.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
Iris-DM
Associate III

OK. In the meantime, can you find out which file/script is called when the generate file button is pressed? I'll see if I can trace through to see where the issue occurs.


@Iris-DM wrote:

OK. In the meantime, can you find out which file/script is called when the generate file button is pressed? I'll see if I can trace through to see where the issue occurs.


@JohanAstrup if you could help on this please..
To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.