2020-03-05 6:17 PM
Does TouchGFX support the "STM32H745I_DISCO" development board?
I tried to build the "STM32H745I_DISCO" project in the latest version STM32Cube V5.6.0, but I couldn't choose TouchGFX as my graphics system. But if I choose other boards, such as ST32F746G_DISCO or STM32H750B_Discovery, I can use TouchGFX. Does TouchGFX not support "STM32H745I_DISCO" development board? Or am I setting something wrong?
2020-03-06 1:04 AM
Reassigned to topic "STM32 MCUs" STM32F7" to reach relevant community.
Olivier
2020-03-06 5:15 AM
Hello CGong,
First of all, it is not possible to add additional software as TouchGFX in CubeMX for H7 dual cores. This will be fixed in the future. Please note that this does not mean that you are not able to use TouchGFX on STM32H745DISCO. In TouchGFX Designer we do not provide and official application template for this board, but it is available on demand.
Please write me soren.mikkelsen@st.com for more information.
Br
Soren