2020-02-26 04:41 AM
I have just spent two days configuring STM32F746GDISCOVERY graphic application via CUBEMX an finally get it work. So I'm sharing my steps.
It is written for dummies like me
Many thanks to Martin Kjeldsen for background information.
There are DOCx, RARed images, ioc file and whole project in the attachmments.
Edit: I should have mentioned that all the code added to main.c and other settings are from project generated by TouchGFX Designer.
Edit2: QUAD SPI is not configured corretly, here is the roght configuration in the video:
2020-03-12 12:56 AM
Yes, STM32F746G-DISCOVERY. QSPI is only needed for storing large images if the controller's FLASH memory is not enough?
I figured it out.
Deleted #include <stm32746g_discovery_qspi.h> from STM32CCubeIDE -> Project -> Core -> main.c
Deleted "stm32746g_discovery_qspi.c" and "stm32746g_discovery_qspi.h" from STM32CCubeIDE->Project->Drivers->BSP
Deleted "n25q128a" from STM32CCubeIDE->Project->Drivers->BSP->Components
2020-03-12 01:37 AM
Great. I have just figured out that I actually didn't used QSPI :)
Here is everything in the video: