2020-02-26 04:41 AM
I have just spent two days configuring STM32F746GDISCOVERY graphic application via CUBEMX an finally get it work. So I'm sharing my steps.
It is written for dummies like me =)
Many thanks to Martin Kjeldsen for background information.
There are DOCx, RARed images, ioc file and whole project in the attachmments.
Edit: I should have mentioned that all the code added to main.c and other settings are from project generated by TouchGFX Designer.
Edit2: QUAD SPI is not configured corretly, here is the roght configuration in the video:
2020-02-27 06:54 AM
You're definitely not a dummy if you can do something like this! <3
/Martin
2020-02-27 09:56 AM
Wow, I really wish I would have gotten the STM32F746GDISCO instead of the 32f7508. This ALMOST works for me. the 7508 is finally using the memory but I am getting a "Break at address "0x800619e" with no debug information available" hmphfff...
2020-02-27 10:12 PM
Very nice, thank you. This should be stickied!
2020-03-09 05:41 AM
Thanks a lot Martin!
2020-03-09 05:44 AM
32f7508 is the similar, but older one, right? Ia have simillar problem with older STM32F429-DISCOVERY. The newer STM32F429-DISC1 works fine.
2020-03-11 12:18 AM
Is it possible to do the same without QSPI?
2020-03-11 06:55 AM
I think there shouldn't be any problem. I'm working at STM32F429 + TouchGFX + VGA display + USB Mouse and it works like a charm at 800×600 without QSPI.
2020-03-11 07:57 AM
Can you tell me how to configure TouchGFX to work without QSPI? All I could do was to spoil the program.
2020-03-12 12:14 AM
What MCU or board? STM32F746 I suppose? Do you have working project WITH QadSPI?