2020-02-20 06:01 PM
I was reading in there reference manual and I found this section: 34.4.2 Supported resolutions and frame rates. But it is noted clear to me I'd I would be able to run a display with 1280×720 resolution?
Is this possible?s
2023-12-16 11:51 PM
Here is TouchGFX , running on SAMSUNG TAB3 10.1 inch ,, 1280x800 , LVDS TFT .
(STM32H745XIT6 + SN75LVDS83B). Its on-going proto type testing project.
All Gauges are custom designed by me.
2023-12-17 06:02 AM
Hi ..
here is my custom designed board with STM32H745XIT6 (Dual-Core).
It is specially designed for TouchGFX related developments.
Its modular type dev board and presently RGB to LVDS board is attached on top left.
Here is SAMSUNG Tab3 7 inch (1024x600) TFT with my new dev board running TouchGFX 😁😎😎😎
Many More ....
2023-12-19 08:34 AM
Thank you for sharing these, very interesting.
2023-12-19 09:06 AM
Hi @ferro . thanks
I have many more to share like below.
if you wish , I can share through private message.
Also working with iPad 12 inch TFT .
Regards
INaee.1
2024-06-25 09:49 PM
How can i change display on STM32H735 can you please help I have to use 7 to 10 inch screen
2024-06-25 10:36 PM
Hi ,,
Yes I can help you .
I have lot of experience in STM32 & TouchGFX
here is my latest TouchGFX Board with STM32H745 & 2.95" , 854X480 TFT.
The PCB has 4 layers .
The board has Modbus RTU Master over same usb cable and I can simulate values on TFT.
regards
I.Naeem
2024-06-26 01:05 AM
Hi, I just want to know how I can change the screen in my existing STM32H735 board as I don't have much time for making new PCB I am having STM32H735 discovery kit
2024-06-26 02:37 AM
Hi contact me privately .. and send me the MX project file and the datasheet of the tft you want to interface
I.N
2024-08-12 10:33 AM
Hi @ferro ...
Here is my latest TouchGFX Experiment with Standard FHD LCD Monitor .
My H745 Dev-board connected to standard lcd over VGA cable and above is the result.
STM32H745 >> ADV7123 >> VGA-CABLE >> FHD-MONITOR 😁😁😁😎😎😎
Regards
I.N
2024-08-12 10:51 AM - edited 2024-08-12 10:53 AM
Your modular design is an excellent approach.
More details on the VGA card please..
BridgeTek? https://brtchip.com/wp-content/uploads/Support/Documentation/Datasheets/ICs/EVE/DS_BT815_6.pdf
Sorry, missed the ADV7123 reference, that DAC's got some head room
https://www.analog.com/en/products/adv7123.html