2020-08-12 10:53 AM
When I add the unicode to the proper font for chinese characters the file gets overwritten when I generate code with TouchGFX. So how do I properly update the fonts this way in the middle of a large project?
2020-08-24 7:25 AM
Hello,
Sorry, I have a hard time understanding your problem.
Are you using your own Chinese font and it gets overwritten ?
You are basically trying to use a Chinese font right ?
Could you elaborate ?
Also, if it is something related to TouchGFX, be sure to add TouchGFX as the topic of the post, otherwise we might not see it.
/Alexandre